2024-02-22 5:28 AM
Hello.
I want to integrate ADC with DMA, and calculate the average count of all convertions.
I'm using the following code:
In adc.c:
```
if(HAL_ADC_PollForConversion(&hadc1, 10) == HAL_OK) {
uint16_t value = HAL_ADC_GetValue(&hadc1);
USART_Send("%.3f", value);
HAL_ADC_Start(&hadc1);
}
```
In main.c:
```
HAL_ADC_Start_DMA(&hadc1, (uint8_t*) AVG_BUF, AVG_BUF_SIZE);
```
However HAL_ADC_GetValue() seems to not use DMA.
I want it to explicitely use DMA to read.
Solved! Go to Solution.
2024-02-22 5:40 AM
HAL_ADC_Start_DMA will put values into the buffer you specify, in this case AVG_BUG. So that is where you should read values from. Implement the HAL_ADC_ConvCpltCallback call to read out the values after they're all transferred. Refer to the documentaiton in stm32f4xx_hal_adc.c:
(++) ADC conversion with transfer by DMA:
(+++) Activate the ADC peripheral and start conversions
using function HAL_ADC_Start_DMA()
(+++) Wait for ADC conversion completion by call of function
HAL_ADC_ConvCpltCallback() or HAL_ADC_ConvHalfCpltCallback()
(these functions must be implemented in user program)
(+++) Conversion results are automatically transferred by DMA into
destination variable address.
(+++) Stop conversion and disable the ADC peripheral
using function HAL_ADC_Stop_DMA()
2024-02-22 5:40 AM
HAL_ADC_Start_DMA will put values into the buffer you specify, in this case AVG_BUG. So that is where you should read values from. Implement the HAL_ADC_ConvCpltCallback call to read out the values after they're all transferred. Refer to the documentaiton in stm32f4xx_hal_adc.c:
(++) ADC conversion with transfer by DMA:
(+++) Activate the ADC peripheral and start conversions
using function HAL_ADC_Start_DMA()
(+++) Wait for ADC conversion completion by call of function
HAL_ADC_ConvCpltCallback() or HAL_ADC_ConvHalfCpltCallback()
(these functions must be implemented in user program)
(+++) Conversion results are automatically transferred by DMA into
destination variable address.
(+++) Stop conversion and disable the ADC peripheral
using function HAL_ADC_Stop_DMA()
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.