2013-03-25 2:18 PM
Hi i
would like
to use the circuit
MAX3232
(
RS232adapter
) to connect twoPORT
RS232
with this
circuit
using just
TX and RX
only
if possible
this experience?
??
??
and thank you2013-03-25 3:02 PM
There seems to be a language barrier here. Perhaps it would be easier to explain your requirement with a diagram...?
2013-03-25 4:15 PM
Here is a
that
represents
my problem
if
possible to do this
configuration?
?? ________________ Attachments : Doc1.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1An&d=%2Fa%2F0X0000000bjO%2FMxvFcOji_FYohzLHw5WB39F3L3WIkazQ.unp2P0.vmY&asPdf=false2013-03-25 11:47 PM
By ''STM32-P103'' I assume you mean this:
https://www.olimex.com/Products/ARM/ST/STM32-P103/
Note that it has one RS232 port already - so you only need to add one other. Study the documentation to see where the other UART port pins can be accessed on the various connectors on the board...2013-03-26 1:31 AM
I see you have also posted the same question in a different thread:
/519d41ef
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.