2026-03-18 12:51 AM
Hi
I'm create a project that sending data from RFID reader (RS232) to PC (via USB HID) as a keyboard.
I using RS232 to TTL for STM32 can read data and using USB HID to send it to PC.
My code is working but a character sending is slow, but when i remove delay, character is missing.
Ex: data from RFID: 4F002F144E
When I have 15ms delay, my PC receive all character
But when remove 15ms, some character is miss.
So I want to ask have anyway to speedup ?
This is my loop:
while (RingBuffer_Availabel(&ring)) {
uint8_t data;
RingBuffer_Pop(&ring, &data);
if(data == '\r'){
send_enter();
break;
}
keyboardhid.MODIFIER = (data >= 'A' && data <= 'Z') ? 0x02 : 0x00;
keyboardhid.KEYCODE1 = ascii_to_hid((char) data);
USBD_HID_SendReport(&hUsbDeviceFS, (uint8_t*) &keyboardhid,sizeof(keyboardhid));
HAL_Delay(15);
usb_ready = 0;
keyboardhid.MODIFIER = 0x00;
keyboardhid.KEYCODE1 = 0x00;
USBD_HID_SendReport(&hUsbDeviceFS, (uint8_t*) &keyboardhid,sizeof(keyboardhid));
HAL_Delay(15);
}
2026-03-18 2:09 AM - edited 2026-03-18 2:10 AM
You must check if the previous operation was completed before starting the next one. I don't use HAL-based USB stack but there surely must be some callback on operation complete and/or HID class structure member for signaling the ready state.
Also, SendReport should be called from an ISR of the same priority as USB interrupt, otherwise it will hang the USB stack at some point.
2026-03-18 5:10 AM
Hello @QuocAn
To ensure minimal delay and improve throughput, use the USB status from the following enumeration
typedef enum
{
USBD_OK = 0U,
USBD_BUSY,
USBD_EMEM,
USBD_FAIL,
} USBD_StatusTypeDef;
as a checkpoint between
USBD_HID_SendReport
Use USBD_StatusTypeDef as a checkpoint between calls to USBD_HID_SendReport.This ensure that the next buffer is sent only when just the USB controller completes the previous transmission and returns USBD_OK.
here is a general view of the algorythm that you can use .
do
{
status = USBD_HID_SendReport(&hUsbDeviceFS, next_report, len);
/* loop until the USB stack accepts the request (USBD_OK) */
}
while (status != USBD_OK);
BR
Gyessine
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.