2023-04-26 4:07 AM
For example, I wish to use ADC1 (14 bits max) of STM32U575 at 12 bits, single ended. The datasheet guarantees a minimum of 68 dB for the SINAD, does this figure get reduced from 14 bits to 12 bits? If so, by how much?
Thanks,
Joel
Solved! Go to Solution.
2023-04-28 11:55 PM
yes, basically your right.
2023-04-28 7:04 AM
Hi @JHIEB.1
The forum moderator had marked your post as needing a little more investigation and direct support. An online support case has been created on your behalf, please stand by for just a moment and you will hear from us.
Regards,
Billy
2023-04-28 2:28 PM
Hi again,
I did some digging on the topic and the answer seems quite simple: If I set the resolution to 12 bits, the SNR for an ideal ADC should be 12x6.02+1.76 = 74 dB, which is clearly more than the 68 dB min SINAD figure, so I won't lose any accuracy by doing so. Actually, as long as the resolution is at least equal to the worst case ENOB, I won't lose any (AC) accuracy. Can anybody confirm?
Thanks,
Joel
2023-04-28 11:55 PM
yes, basically your right.
2023-04-29 11:37 AM
Thanks!
2023-04-29 12:24 PM
> on average, the 14b data should have lower noise
You can capture or add how many bits you want, but the data cannot have a lower noise than the ENOB.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.