2024-09-18 11:05 AM
The thing is,i have a custom design board with STM32F446RE and it's Nucleo variant
i have a code with multiple timers but when i run the program on my custom board it goes to Hardfault error after a timer callback but the same problem dosent happens with the Nucleo board although the code remains the same
Solved! Go to Solution.
2024-09-18 11:30 AM
Don't discount bad design
Make sure clock expectations are the same, make sure VCAP capacitors are correctly rated as designed/populated. You've got 4u7 F between them, and see 1.25V
Check FLASH wait states.
Root Cause the HARD FAULT, with a handler that does a better job than while(1) silently dying.
2024-09-18 11:12 AM
Hello @Nirbhik and welcome to the community.
@Nirbhik wrote:
The thing is,i have a custom design board with STM32F446RE and it's Nucleo variant.
What do you mean by variant. is it Blue/Black pill board?
Do you have the same Clock source and frequency values?
2024-09-18 11:30 AM
Don't discount bad design
Make sure clock expectations are the same, make sure VCAP capacitors are correctly rated as designed/populated. You've got 4u7 F between them, and see 1.25V
Check FLASH wait states.
Root Cause the HARD FAULT, with a handler that does a better job than while(1) silently dying.
2024-09-18 7:25 PM - edited 2024-09-18 7:38 PM
Yes i hadn't placed a capacitor at the Vcap pin
also about your last statement
"Root Cause the HARD FAULT, with a handler that does a better job than while(1) silently dying."
i use the debug tools of ST and i was able to pinpoint the error because of the call stack whose image i am attaching below
2024-09-18 7:26 PM
i have the NUCLEO-F446RE and yes i have the same clock source as i am using the same clock based on the internal oscillator
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.