2020-07-24 1:33 PM
Helllo,
I'm working on the NUCLEO-F722ZE EVB.
I want my code to wait for a character to be received from UART 3 and do nothing.
This is what I wrote:
unibt8_t received_character = 0 ;
HAL_UART_Receive(&huart3, received_character, 1,1000) ;From what I understand "HAL_UART_Receive" is a blocking function so it should block the code execution until a character is received. But for some reason my code doesn't stop and proceeds to the next line although no data was sent to the UART.
What am I doing wrong ?
2020-07-24 1:39 PM
> until a character is received.
Or until the timeout occurs. You have specified a 1000ms timeout.
The return value will be HAL_TIMEOUT in this case, which you can catch and handle appropriately.
2020-07-24 1:42 PM
How can I make it wait indefinitely ?
2020-07-24 2:00 PM
0xFFFFFFFE gives you a timeout of 50 days.
Otherwise you need a loop:
while (HAL_UART_Receive(&huart3, &received_character, 1, 1000) == HAL_TIMEOUT);Your code also has typos.
unibt8_t received_character = 0 ; // <-- unibt8_t is not a type
HAL_UART_Receive(&huart3, received_character, 1,1000) ; // <-- this writes to memory address 0. missing a & character
2020-07-24 3:52 PM
Thanks.
What did you mean by:
"<-- unibt8_t is not a type" ?
2020-07-24 11:18 PM
Unless you really do expect only a single byte, I would strongly recommend at least to use interrupts which anyway are part of normal practice in microcontroller world. If you don't want interrupts and don't care the latency, use DMA with cyclic buffer (say 1024 bytes) so you can see what you receive in the buffer. Size the buffer so that its size don't overflow with the worst case polling delay.
2020-07-25 4:25 AM
Yes, I get your point.
But for this peripheral - the single byte is a requirement.
I want the user to press on a single keyboard character to navigate in an internal menu.
I have another UART in the design that's intended to send/receive chunks of data with another device.
For that UART it'll probably be wise to use a DMA.
Are there official ST examples that showcase the usage of HAL functions ?
2020-07-25 6:01 AM
Go for interrupts and fill up the callback isr portion. That's futureproof. In polling monitor for the rxne flag prior to read the data byte.
2020-07-25 6:34 AM
Can you please post an example for this ?
2020-07-25 10:19 AM
> Are there official ST examples that showcase the usage of HAL functions ?
Here are three of many:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.