2020-10-21 11:00 AM
But yet it is called for HAL_QSPI_Transmit_DMA function? Do I need to configure the autopolling with the QSPI_AutoPollingTypeDef structure for the callback to be called with the HAL_QSPI_Transmit function?
2020-10-21 11:35 AM
It's not called in blocking mode, since the transmit is complete when the function returns. In interrupt/DMA mode, this isn't the case.
Instructions for the HAL functions are at the top of the source file:
(#) For the indirect write mode, use HAL_QSPI_Transmit(), HAL_QSPI_Transmit_DMA() or
HAL_QSPI_Transmit_IT() after the command configuration :
(++) In polling mode, the output of the function is done when the transfer is complete.
(++) In interrupt mode, HAL_QSPI_FifoThresholdCallback() will be called when the fifo threshold
is reached and HAL_QSPI_TxCpltCallback() will be called when the transfer is complete.
(++) In DMA mode, HAL_QSPI_TxHalfCpltCallback() will be called at the half transfer and
HAL_QSPI_TxCpltCallback() will be called when the transfer is complete.
2020-10-21 11:50 AM
Thank you. I'll look at this a little later. Is it the same for the HAL_QSPI_Receive function?
2020-10-22 10:36 AM
Never mind, I see that it applies to the HAL_QSPI_Receive as well. Thanks for your help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.