2024-12-03 4:54 AM
Hello,
I am working on interfacing an external flash memory IC MT25QL512 with the STM32H745 microcontroller using QSPI in IAR Embedded Workbench.
When attempting to write data to the external flash using the HAL_QSPI_Transmit function, the operation fails at the following line:
status = QSPI_WaitFlagStateUntilTimeout(hqspi, QSPI_FLAG_TC, SET, tickstart, Timeout);
Thank you for your support!!
Solved! Go to Solution.
2024-12-03 5:22 AM - edited 2024-12-03 5:23 AM
Hard to say, you're pushing the content, so should have control of the speed of the transaction.
Are you placing a Debug View of the QSPI Peripheral Registers? Should probably avoid that due to secondary effects of the debugger, the status registers, and the data/FIFO registers.
Anything else trying to operate concurrently with the memory?
Able to get a logic analyzer on the pins?
Other code examples working? Clock/Peripheral enabled? ie non-zero content in registers and writable.
2024-12-03 5:22 AM - edited 2024-12-03 5:23 AM
Hard to say, you're pushing the content, so should have control of the speed of the transaction.
Are you placing a Debug View of the QSPI Peripheral Registers? Should probably avoid that due to secondary effects of the debugger, the status registers, and the data/FIFO registers.
Anything else trying to operate concurrently with the memory?
Able to get a logic analyzer on the pins?
Other code examples working? Clock/Peripheral enabled? ie non-zero content in registers and writable.
2024-12-03 9:10 PM
Attached IAR debug logs
0.001: File generated Wed Dec 4 10:36:52 2024
0.000: Pass 3 of 3
0.000: Starting fragment-style flashloader pass.
0.000: Device: C:\Users\harshal.gajjalwar\Desktop\External_IAR_LODER\FlashSTM32H745I-DISCO_QSPI_test.flash
0.001: Flash loader: C:\Users\harshal.gajjalwar\Desktop\External_IAR_LODER\FlashSTM32H7xx_QSPI_MICRON.out
0.154: FlashInitEntry is at 0x2400'25f4
0.154: FlashWriteEntry is at 0x2400'25fc
0.154: FlashEraseWriteEntry is at 0x2400'2604
0.154: FlashBreak is at 0x2400'00f8
0.154: FlashBufferStart is at 0x2400'4800
0.154: FlashBufferEnd is at 0x2404'0000
0.154: theFlashParams is at 0x2400'2644
0.154: FlashPreInitEntry not found
0.156: FlashChecksumEntry not found
0.156: FlashSignoffEntry not found
0.156: page size is 256 (0x100)
0.156: filler is 0xff
0.156: buffer size is 243712 (0x3'b800) 0.156:
0.156: Base of flash at 0x9000'0000
0.156: SimpleCode records (after offset):
0.156: Record 0: @ 0x9000'0000 [6824272 (0x68'2150) bytes] 0x9000'0000 - 0x9068'214f [0 0 0 0 ... ]
0.156: ->init : base @ 0x9000'0000, image size 0x68'2150
0.156: Store TargetParams to 0x2400'2644
0.157: Setting PC to 0x2400'25f4 (FlashInitEntry)
0.196: timing(init): 0.0000 (CPU) 0.0310 (elapsed)
0.196: Load TargetParams from 0x2400'2644
0.199: Transaction list:
0.199: Transaction 0: @ 0x9000'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9000'0000 (0x1'0000 bytes)
0.199: 1: 0x9001'0000 (0x1'0000 bytes)
0.199: 2: 0x9002'0000 (0x1'0000 bytes)
0.199: Transaction 1: @ 0x9003'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9003'0000 (0x1'0000 bytes)
0.199: 1: 0x9004'0000 (0x1'0000 bytes)
0.199: 2: 0x9005'0000 (0x1'0000 bytes)
0.199: Transaction 2: @ 0x9006'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9006'0000 (0x1'0000 bytes)
0.199: 1: 0x9007'0000 (0x1'0000 bytes)
0.199: 2: 0x9008'0000 (0x1'0000 bytes)
0.199: Transaction 3: @ 0x9009'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9009'0000 (0x1'0000 bytes)
0.199: 1: 0x900a'0000 (0x1'0000 bytes)
0.199: 2: 0x900b'0000 (0x1'0000 bytes)
0.199: Transaction 4: @ 0x900c'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x900c'0000 (0x1'0000 bytes)
0.199: 1: 0x900d'0000 (0x1'0000 bytes)
0.199: 2: 0x900e'0000 (0x1'0000 bytes)
0.199: Transaction 5: @ 0x900f'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x900f'0000 (0x1'0000 bytes)
0.199: 1: 0x9010'0000 (0x1'0000 bytes)
0.199: 2: 0x9011'0000 (0x1'0000 bytes)
0.199: Transaction 6: @ 0x9012'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9012'0000 (0x1'0000 bytes)
0.199: 1: 0x9013'0000 (0x1'0000 bytes)
0.199: 2: 0x9014'0000 (0x1'0000 bytes)
0.199: Transaction 7: @ 0x9015'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9015'0000 (0x1'0000 bytes)
0.199: 1: 0x9016'0000 (0x1'0000 bytes)
0.199: 2: 0x9017'0000 (0x1'0000 bytes)
0.199: Transaction 8: @ 0x9018'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9018'0000 (0x1'0000 bytes)
0.199: 1: 0x9019'0000 (0x1'0000 bytes)
0.199: 2: 0x901a'0000 (0x1'0000 bytes)
0.199: Transaction 9: @ 0x901b'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x901b'0000 (0x1'0000 bytes)
0.199: 1: 0x901c'0000 (0x1'0000 bytes)
0.199: 2: 0x901d'0000 (0x1'0000 bytes)
0.199: Transaction 10: @ 0x901e'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x901e'0000 (0x1'0000 bytes)
0.199: 1: 0x901f'0000 (0x1'0000 bytes)
0.199: 2: 0x9020'0000 (0x1'0000 bytes)
0.199: Transaction 11: @ 0x9021'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9021'0000 (0x1'0000 bytes)
0.199: 1: 0x9022'0000 (0x1'0000 bytes)
0.199: 2: 0x9023'0000 (0x1'0000 bytes)
0.199: Transaction 12: @ 0x9024'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9024'0000 (0x1'0000 bytes)
0.199: 1: 0x9025'0000 (0x1'0000 bytes)
0.199: 2: 0x9026'0000 (0x1'0000 bytes)
0.199: Transaction 13: @ 0x9027'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9027'0000 (0x1'0000 bytes)
0.199: 1: 0x9028'0000 (0x1'0000 bytes)
0.199: 2: 0x9029'0000 (0x1'0000 bytes)
0.199: Transaction 14: @ 0x902a'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x902a'0000 (0x1'0000 bytes)
0.199: 1: 0x902b'0000 (0x1'0000 bytes)
0.199: 2: 0x902c'0000 (0x1'0000 bytes)
0.199: Transaction 15: @ 0x902d'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x902d'0000 (0x1'0000 bytes)
0.199: 1: 0x902e'0000 (0x1'0000 bytes)
0.199: 2: 0x902f'0000 (0x1'0000 bytes)
0.199: Transaction 16: @ 0x9030'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9030'0000 (0x1'0000 bytes)
0.199: 1: 0x9031'0000 (0x1'0000 bytes)
0.199: 2: 0x9032'0000 (0x1'0000 bytes)
0.199: Transaction 17: @ 0x9033'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9033'0000 (0x1'0000 bytes)
0.199: 1: 0x9034'0000 (0x1'0000 bytes)
0.199: 2: 0x9035'0000 (0x1'0000 bytes)
0.199: Transaction 18: @ 0x9036'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9036'0000 (0x1'0000 bytes)
0.199: 1: 0x9037'0000 (0x1'0000 bytes)
0.199: 2: 0x9038'0000 (0x1'0000 bytes)
0.199: Transaction 19: @ 0x9039'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9039'0000 (0x1'0000 bytes)
0.199: 1: 0x903a'0000 (0x1'0000 bytes)
0.199: 2: 0x903b'0000 (0x1'0000 bytes)
0.199: Transaction 20: @ 0x903c'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x903c'0000 (0x1'0000 bytes)
0.199: 1: 0x903d'0000 (0x1'0000 bytes)
0.199: 2: 0x903e'0000 (0x1'0000 bytes)
0.199: Transaction 21: @ 0x903f'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x903f'0000 (0x1'0000 bytes)
0.199: 1: 0x9040'0000 (0x1'0000 bytes)
0.199: 2: 0x9041'0000 (0x1'0000 bytes)
0.199: Transaction 22: @ 0x9042'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9042'0000 (0x1'0000 bytes)
0.199: 1: 0x9043'0000 (0x1'0000 bytes)
0.199: 2: 0x9044'0000 (0x1'0000 bytes)
0.199: Transaction 23: @ 0x9045'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9045'0000 (0x1'0000 bytes)
0.200: 1: 0x9046'0000 (0x1'0000 bytes)
0.200: 2: 0x9047'0000 (0x1'0000 bytes)
0.200: Transaction 24: @ 0x9048'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.200: Will erase 3 block(s):
0.200: 0: 0x9048'0000 (0x1'0000 bytes)
0.200: 1: 0x9049'0000 (0x1'0000 bytes)
0.200: 2: 0x904a'0000 (0x1'0000 bytes)
0.200: Transaction 25: @ 0x904b'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.200: Will erase 3 block(s):
0.200: 0: 0x904b'0000 (0x1'0000 bytes)
0.200: 1: 0x904c'0000 (0x1'0000 bytes)
0.200: 2: 0x904d'0000 (0x1'0000 bytes)
0.200: Transaction 26: @ 0x904e'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.200: Will erase 3 block(s):
0.200: 0: 0x904e'0000 (0x1'0000 bytes)
0.200: 1: 0x904f'0000 (0x1'0000 bytes)
0.200: 2: 0x9050'0000 (0x1'0000 bytes)
0.200: Transaction 27: @ 0x9051'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.200: Will erase 3 block(s):
0.200: 0: 0x9051'0000 (0x1'0000 bytes)
0.200: 1: 0x9052'0000 (0x1'0000 bytes)
0.200: 2: 0x9053'0000 (0x1'0000 bytes)
0.200: Transaction 28: @ 0x9054'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.200: Will erase 3 block(s):
0.200: 0: 0x9054'0000 (0x1'0000 bytes)
0.200: 1: 0x9055'0000 (0x1'0000 bytes)
0.200: 2: 0x9056'0000 (0x1'0000 bytes)
0.200: Transaction 29: @ 0x9057'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.200: Will erase 3 block(s):
0.200: 0: 0x9057'0000 (0x1'0000 bytes)
0.200: 1: 0x9058'0000 (0x1'0000 bytes)
0.200: 2: 0x9059'0000 (0x1'0000 bytes)
0.200: Transaction 30: @ 0x905a'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.200: Will erase 3 block(s):
0.200: 0: 0x905a'0000 (0x1'0000 bytes)
0.200: 1: 0x905b'0000 (0x1'0000 bytes)
0.200: 2: 0x905c'0000 (0x1'0000 bytes)
0.200: Transaction 31: @ 0x905d'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.200: Will erase 3 block(s):
0.200: 0: 0x905d'0000 (0x1'0000 bytes)
0.200: 1: 0x905e'0000 (0x1'0000 bytes)
0.200: 2: 0x905f'0000 (0x1'0000 bytes)
0.200: Transaction 32: @ 0x9060'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.200: Will erase 3 block(s):
0.200: 0: 0x9060'0000 (0x1'0000 bytes)
0.200: 1: 0x9061'0000 (0x1'0000 bytes)
0.200: 2: 0x9062'0000 (0x1'0000 bytes)
0.200: Transaction 33: @ 0x9063'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.200: Will erase 3 block(s):
0.200: 0: 0x9063'0000 (0x1'0000 bytes)
0.200: 1: 0x9064'0000 (0x1'0000 bytes)
0.200: 2: 0x9065'0000 (0x1'0000 bytes)
0.200: Transaction 34: @ 0x9066'0000 + 0x0 (0x2'2200=139776 bytes) 3 packet(s).
0.200: Will erase 3 block(s):
0.200: 0: 0x9066'0000 (0x1'0000 bytes)
0.200: 1: 0x9067'0000 (0x1'0000 bytes)
0.200: 2: 0x9068'0000 (0x1'0000 bytes)
0.222: ->multi_erase: 3 blocks (0x18 bytes in buffer) [0 0 0]
0.223: Store TargetParams to 0x2400'2644
0.224: Setting PC to 0x2400'2604 (FlashEraseWriteEntry)
0.273: timing(erase): 0.0000 (CPU) 0.0410 (elapsed)
0.274: Load TargetParams from 0x2400'2644
0.274: ->write : @ 0x9000'0000 (0x3'0000 bytes, offset 0x0 into block @ 0x9000'0000) [0 0 0]
0.274: Writing 0x3'0000 bytes to FlashBuffer @ 0x2400'4800
1.793: Store TargetParams to 0x2400'2644
1.795: Setting PC to 0x2400'25fc (FlashWriteEntry)
1.842: timing(write): 0.0000 (CPU) 0.0370 (elapsed)
1.842: Load TargetParams from 0x2400'2644
1.845: Func returned 4 (0 means Ok) 630_d_90000000
1.873: Flash loading pass finished
2024-12-05 1:38 AM
Hello @Harsh_Gajjalwar ,
You have selected Tesla's answer as "best solution".
Where you able to fix your issue?
Regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.