2017-06-26 12:23 AM
Hello. I have custom serial bootloader, which located in the beginning of user flash (sector0), and also user application, which burned by bootloader starting from sector 1 (slightly modified IAP example from ST). While in user app, I want to perform software reset to restart from my custom bootloader. The problem is, if I call HAL_NVIC_SystemReset(), my application just freeze. Also I tried IWDT reset with IWDG_Enable() with same result. Hardware reset from NRST pin working just fine. Also, if I call
HAL_NVIC_SystemReset while in bootloader, reset working OK also. NRST pin connected to ground via 0.1 cap. No external pull-ups or anything.
#stm32f410rb #stm32 #reset2019-03-05 11:53 AM
Did you end up resolving this issue?
2019-03-05 12:02 PM
Make sure BOOT0 is pulled low to ensure your code is entered in FLASH, and not ROM.
Make sure NRST is NOT driven high by some other external push-pull driver.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.