STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Handling 16bit register address in i2c communication

I am trying to use ov5640 camera with stm32l4r5 board nucleo-144. The ov5640 has SCCB bus which is similar to i2c. But ov5640 has register with 16bit address (0x300A, 0x300B like this). I used CUBEMX to initialise i2c pins and generated code. How can...

PToma.14 by Associate II
  • 2390 Views
  • 2 replies
  • 0 kudos

Resolved! ADC resolution and its reference voltage

I am using STM32F407VG board. I wanted to know about the reference voltage and ADC resolution available on this board. I couldn't find the exact info related to these parameters in the datasheets.

rrach by Associate II
  • 1721 Views
  • 2 replies
  • 0 kudos

Advancing debug steps clock by clock

Hello AllI understand that debug steps advance instruction by instruction (whether in C or assembly). I wonder if there is any way to advance CPU clock by CPU clock. I need this to debug an issue I have with the SysTick timer.Thanks

Amir1 by Associate II
  • 1316 Views
  • 5 replies
  • 0 kudos

Resolved! STM32L0 stop mode - RTC wakeup not working after RESET

STM32L041F6 - I configured RTC for wakeup every second from Stop mode. It works ok, but after external reset (NRST pin) it not working. Program run in main while() only once, to line:HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);...

mat-ush by Associate
  • 2280 Views
  • 1 replies
  • 0 kudos

fast ADC and fast clock in the same chip?

The STM32L4xx have excellent 4.5~5MSa/s simultaneous sampling ADC but abysmal 80 MHz CPU clocks. The fast STM32F's have faster clocks but ADC are <2.5Msps. Is there no MCU with 5Msps ADC and 200MHz+ CPU clock?

jandle by Associate
  • 1179 Views
  • 2 replies
  • 1 kudos

Nucleo64 - default blinky description

UM1724 rev.12, in chapter 5.1 Getting started in description of the default blinky program which comes preprogrammed with the board, says:5. Observe the blinking frequency of the three LEDs LD1 to LD3, by clicking on the buttonB1.What?LD1 is STLink's...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.