2016-11-03 7:39 AM
Hi,
__HAL_LOCK has never bothered us previously with v 1.3 HAL library.However, I have updated to 1.5.1 STM32F7 lib and found that stm32f7xx_hal_sai caused us problems.It was related to the handle being kept locked after calling HAL_SAI_DMAStop when no DMA transfer was already happening. (ie, hdma->Lock = HAL_LOCKED)I notice there are lots of routines which lock the SAI handle, yet return without unlocking. Shouldn't all return paths unlock the handle ??For example:HAL_StatusTypeDef HAL_SAI_DMAStop(SAI_HandleTypeDef *hsai){ /* Process Locked */ __HAL_LOCK(hsai); /* Disable the SAI DMA request */ hsai->Instance->CR1 &= ~SAI_xCR1_DMAEN; /* Abort the SAI DMA Streams */ if(hsai->hdmatx != NULL) { if(HAL_DMA_Abort(hsai->hdmatx) != HAL_OK) { // SHOULD INSERT THIS HERE ????? __HAL_UNLOCK(hsai); return HAL_ERROR; } } if(hsai->hdmarx != NULL) { if(HAL_DMA_Abort(hsai->hdmarx) != HAL_OK) { // SHOULD INSERT THIS HERE ????? __HAL_UNLOCK(hsai); return HAL_ERROR; } } /* Disable SAI peripheral */ SAI_Disable(hsai); hsai->State = HAL_SAI_STATE_READY; /* Process Unlocked */ __HAL_UNLOCK(hsai); return HAL_OK;} #stm32f7 #dogfooding2016-11-03 9:00 AM
Shouldn't all return paths unlock the handle ??
You'd think, but the library is disappointingly poor in its implementation and testing.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.