STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BackColor and transparency

Posted on November 04, 2016 at 00:52Hi I make some experiments with the board STM32F469I-Discovery and the examples provided by ST; using the example LCD_DSI_CmdMode_DoubleBuffering I noticed some problem with the transparency with the BackColor of ...

livio by Associate II
  • 762 Views
  • 0 replies
  • 0 kudos

F407 - ADC/DAC at 400 kHz and UART using HAL?

Posted on November 02, 2016 at 13:17Hi all, i think i am experiencing a timing issue here. I configured the STM32F407 using CubeMX and the latest HAL FW Package. I set the clocks to max using HSE (8 MHz) with PLL to run HCLK with 168 MHz and maxed A...

Old discovery stm32F407 with chip rev. A, I2C issue

Posted on November 03, 2016 at 17:18I tried a lot of time generate I2C code with cube MX and AC6 IDE, but I never see SDA or SCL move. I generated code for other I2C than I2C1 but with no success. Is there any issue using stm32f407VGT6 Rev. A mount...

Bug in HAL_SPI_Receive

Posted on October 07, 2016 at 02:31  The original post was too long to process during our migration. Please click on the attachment to read the original post.

shar9393 by Associate
  • 2637 Views
  • 3 replies
  • 0 kudos

problem with USB migrating from stm32f072 to stm32f042

Posted on November 02, 2016 at 22:18I have a USB CDC project that works fine with the STM32F072-DISCO board, but when I try to migrate the code over to my own board with an STM32F042 on it the device shows up as an ''STM Device in DFU Mode'' instead...

hampton by Associate II
  • 1257 Views
  • 2 replies
  • 0 kudos

__HAL_LOCK routines with no __HAL_UNLOCK

Posted on November 03, 2016 at 15:39Hi,__HAL_LOCK has never bothered us previously with v 1.3 HAL library.However, I have updated to 1.5.1 STM32F7 lib and found that stm32f7xx_hal_sai caused us problems.It was related to the handle being kept locked...

AndyJT by Associate III
  • 1167 Views
  • 1 replies
  • 0 kudos

STM32F030 UART TX via DMA only works once

Posted on October 31, 2016 at 22:25 Hi, I've seen similar questions to this but none seem to have helped. I'm transmitting on UART1 via DMA channel 2 and the first transmission works fine. I am unable to get anything out after receiv...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.