2024-08-06 3:02 AM
hello forum
I'm trying to use two examples at once, I'm looking for a script to save an image on an SD card as Jpeg
the examples are:
BSP
JPEG_EncodingUsingFs_DMA
I'm trying to import the JPEG_Encoding example into the BSP one,
While doing so, the compiler doesn't recognize the function JPEG_InitColorTables();
it's part of the jpeg_utils.c under #if (USE_JPEG_ENCODER==1). which I have defined in jpeg_utils_conf.h but the compiler still doesn't recognize it.
am I missing something?
2024-08-07 2:19 AM - edited 2024-08-07 2:21 AM
That's not the full output log!
Go to the 'Console' window, select all, then copy and paste the text here.
Best to post the text as for source code - using the </> button:
2024-08-07 2:26 AM
like that?
12:15:36 **** Incremental Build of configuration Debug for project BSP_CM7 ****
make -j12 all
arm-none-eabi-gcc "C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/audio_play.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DDEBUG -DUSE_STM32H747I_DISCO -DUSE_HAL_DRIVER -DSTM32H747xx -DCORE_CM7 -DTS_MULTI_TOUCH_SUPPORTED -c -I../../../CM7/Inc -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/BSP/STM32H747I-DISCO -I../../../Drivers/BSP/Components/Common -I../../../Utilities/lcd -I../../../Utilities/Fonts -I../../../Utilities/CPU -I../../../Middlewares/ST/STM32_Audio/Addons/PDM/Inc -I../../../Drivers/CMSIS/Include -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM7/Utilities" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM4/Utilities" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/Utilities/lcd" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/fs" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/fs/JPEG" -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Example/User/CM7/audio_play.d" -MT"Example/User/CM7/audio_play.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Example/User/CM7/audio_play.o"
arm-none-eabi-gcc "C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/audio_record.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DDEBUG -DUSE_STM32H747I_DISCO -DUSE_HAL_DRIVER -DSTM32H747xx -DCORE_CM7 -DTS_MULTI_TOUCH_SUPPORTED -c -I../../../CM7/Inc -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/BSP/STM32H747I-DISCO -I../../../Drivers/BSP/Components/Common -I../../../Utilities/lcd -I../../../Utilities/Fonts -I../../../Utilities/CPU -I../../../Middlewares/ST/STM32_Audio/Addons/PDM/Inc -I../../../Drivers/CMSIS/Include -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM7/Utilities" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM4/Utilities" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/Utilities/lcd" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/fs" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/fs/JPEG" -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Example/User/CM7/audio_record.d" -MT"Example/User/CM7/audio_record.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Example/User/CM7/audio_record.o"
arm-none-eabi-gcc "C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/camera.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DDEBUG -DUSE_STM32H747I_DISCO -DUSE_HAL_DRIVER -DSTM32H747xx -DCORE_CM7 -DTS_MULTI_TOUCH_SUPPORTED -c -I../../../CM7/Inc -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/BSP/STM32H747I-DISCO -I../../../Drivers/BSP/Components/Common -I../../../Utilities/lcd -I../../../Utilities/Fonts -I../../../Utilities/CPU -I../../../Middlewares/ST/STM32_Audio/Addons/PDM/Inc -I../../../Drivers/CMSIS/Include -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM7/Utilities" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM4/Utilities" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/Utilities/lcd" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/fs" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/fs/JPEG" -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Example/User/CM7/camera.d" -MT"Example/User/CM7/camera.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Example/User/CM7/camera.o"
arm-none-eabi-gcc "../Example/User/CM7/encode_dma.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DDEBUG -DUSE_STM32H747I_DISCO -DUSE_HAL_DRIVER -DSTM32H747xx -DCORE_CM7 -DTS_MULTI_TOUCH_SUPPORTED -c -I../../../CM7/Inc -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/BSP/STM32H747I-DISCO -I../../../Drivers/BSP/Components/Common -I../../../Utilities/lcd -I../../../Utilities/Fonts -I../../../Utilities/CPU -I../../../Middlewares/ST/STM32_Audio/Addons/PDM/Inc -I../../../Drivers/CMSIS/Include -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM7/Utilities" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM4/Utilities" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/Utilities/lcd" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/fs" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/fs/JPEG" -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Example/User/CM7/encode_dma.d" -MT"Example/User/CM7/encode_dma.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Example/User/CM7/encode_dma.o"
arm-none-eabi-gcc "C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/joystick.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DDEBUG -DUSE_STM32H747I_DISCO -DUSE_HAL_DRIVER -DSTM32H747xx -DCORE_CM7 -DTS_MULTI_TOUCH_SUPPORTED -c -I../../../CM7/Inc -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/BSP/STM32H747I-DISCO -I../../../Drivers/BSP/Components/Common -I../../../Utilities/lcd -I../../../Utilities/Fonts -I../../../Utilities/CPU -I../../../Middlewares/ST/STM32_Audio/Addons/PDM/Inc -I../../../Drivers/CMSIS/Include -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM7/Utilities" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM4/Utilities" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/Utilities/lcd" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/fs" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/fs/JPEG" -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Example/User/CM7/joystick.d" -MT"Example/User/CM7/joystick.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Example/User/CM7/joystick.o"
arm-none-eabi-gcc "C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/lcd.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DDEBUG -DUSE_STM32H747I_DISCO -DUSE_HAL_DRIVER -DSTM32H747xx -DCORE_CM7 -DTS_MULTI_TOUCH_SUPPORTED -c -I../../../CM7/Inc -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/BSP/STM32H747I-DISCO -I../../../Drivers/BSP/Components/Common -I../../../Utilities/lcd -I../../../Utilities/Fonts -I../../../Utilities/CPU -I../../../Middlewares/ST/STM32_Audio/Addons/PDM/Inc -I../../../Drivers/CMSIS/Include -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM7/Utilities" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM4/Utilities" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/Utilities/lcd" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/fs" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/fs/JPEG" -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Example/User/CM7/lcd.d" -MT"Example/User/CM7/lcd.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Example/User/CM7/lcd.o"
arm-none-eabi-gcc "C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/main.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DDEBUG -DUSE_STM32H747I_DISCO -DUSE_HAL_DRIVER -DSTM32H747xx -DCORE_CM7 -DTS_MULTI_TOUCH_SUPPORTED -c -I../../../CM7/Inc -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/BSP/STM32H747I-DISCO -I../../../Drivers/BSP/Components/Common -I../../../Utilities/lcd -I../../../Utilities/Fonts -I../../../Utilities/CPU -I../../../Middlewares/ST/STM32_Audio/Addons/PDM/Inc -I../../../Drivers/CMSIS/Include -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM7/Utilities" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM4/Utilities" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/Utilities/lcd" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/fs" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/fs/JPEG" -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Example/User/CM7/main.d" -MT"Example/User/CM7/main.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Example/User/CM7/main.o"
arm-none-eabi-gcc "C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/qspi.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DDEBUG -DUSE_STM32H747I_DISCO -DUSE_HAL_DRIVER -DSTM32H747xx -DCORE_CM7 -DTS_MULTI_TOUCH_SUPPORTED -c -I../../../CM7/Inc -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/BSP/STM32H747I-DISCO -I../../../Drivers/BSP/Components/Common -I../../../Utilities/lcd -I../../../Utilities/Fonts -I../../../Utilities/CPU -I../../../Middlewares/ST/STM32_Audio/Addons/PDM/Inc -I../../../Drivers/CMSIS/Include -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM7/Utilities" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM4/Utilities" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/Utilities/lcd" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/fs" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/fs/JPEG" -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Example/User/CM7/qspi.d" -MT"Example/User/CM7/qspi.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Example/User/CM7/qspi.o"
arm-none-eabi-gcc "C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/sd.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DDEBUG -DUSE_STM32H747I_DISCO -DUSE_HAL_DRIVER -DSTM32H747xx -DCORE_CM7 -DTS_MULTI_TOUCH_SUPPORTED -c -I../../../CM7/Inc -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/BSP/STM32H747I-DISCO -I../../../Drivers/BSP/Components/Common -I../../../Utilities/lcd -I../../../Utilities/Fonts -I../../../Utilities/CPU -I../../../Middlewares/ST/STM32_Audio/Addons/PDM/Inc -I../../../Drivers/CMSIS/Include -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM7/Utilities" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM4/Utilities" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/Utilities/lcd" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/fs" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/fs/JPEG" -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Example/User/CM7/sd.d" -MT"Example/User/CM7/sd.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Example/User/CM7/sd.o"
arm-none-eabi-gcc "C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/sdram.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DDEBUG -DUSE_STM32H747I_DISCO -DUSE_HAL_DRIVER -DSTM32H747xx -DCORE_CM7 -DTS_MULTI_TOUCH_SUPPORTED -c -I../../../CM7/Inc -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/BSP/STM32H747I-DISCO -I../../../Drivers/BSP/Components/Common -I../../../Utilities/lcd -I../../../Utilities/Fonts -I../../../Utilities/CPU -I../../../Middlewares/ST/STM32_Audio/Addons/PDM/Inc -I../../../Drivers/CMSIS/Include -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM7/Utilities" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM4/Utilities" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/Utilities/lcd" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/fs" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/fs/JPEG" -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Example/User/CM7/sdram.d" -MT"Example/User/CM7/sdram.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Example/User/CM7/sdram.o"
arm-none-eabi-gcc "C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/stm32h7xx_it.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DDEBUG -DUSE_STM32H747I_DISCO -DUSE_HAL_DRIVER -DSTM32H747xx -DCORE_CM7 -DTS_MULTI_TOUCH_SUPPORTED -c -I../../../CM7/Inc -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/BSP/STM32H747I-DISCO -I../../../Drivers/BSP/Components/Common -I../../../Utilities/lcd -I../../../Utilities/Fonts -I../../../Utilities/CPU -I../../../Middlewares/ST/STM32_Audio/Addons/PDM/Inc -I../../../Drivers/CMSIS/Include -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM7/Utilities" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM4/Utilities" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/Utilities/lcd" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/fs" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/fs/JPEG" -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Example/User/CM7/stm32h7xx_it.d" -MT"Example/User/CM7/stm32h7xx_it.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Example/User/CM7/stm32h7xx_it.o"
arm-none-eabi-gcc "C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/touchscreen.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DDEBUG -DUSE_STM32H747I_DISCO -DUSE_HAL_DRIVER -DSTM32H747xx -DCORE_CM7 -DTS_MULTI_TOUCH_SUPPORTED -c -I../../../CM7/Inc -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/BSP/STM32H747I-DISCO -I../../../Drivers/BSP/Components/Common -I../../../Utilities/lcd -I../../../Utilities/Fonts -I../../../Utilities/CPU -I../../../Middlewares/ST/STM32_Audio/Addons/PDM/Inc -I../../../Drivers/CMSIS/Include -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM7/Utilities" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM4/Utilities" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/Utilities/lcd" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/fs" -I"C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/fs/JPEG" -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Example/User/CM7/touchscreen.d" -MT"Example/User/CM7/touchscreen.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Example/User/CM7/touchscreen.o"
../Example/User/CM7/encode_dma.c: In function 'JPEG_Encode_DMA':
../Example/User/CM7/encode_dma.c:113:3: warning: implicit declaration of function 'BMP_GetInfo'; did you mean 'BSP_QSPI_GetInfo'? [-Wimplicit-function-declaration]
113 | BMP_GetInfo(pBmpFile, &Conf);
| ^~~~~~~~~~~
| BSP_QSPI_GetInfo
C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/main.c: In function 'main':
C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/main.c:128:3: warning: statement with no effect [-Wunused-value]
128 | JPEG_InitColorTables;
| ^~~~~~~~~~~~~~~~~~~~
In file included from ../../../Drivers/BSP/STM32H747I-DISCO/stm32h747i_discovery.h:32,
from ../../../CM7/Inc/main.h:30,
from C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/main.c:21:
../../../CM7/Inc/stm32h747i_discovery_conf.h:56:35: warning: passing argument 2 of 'JPEG_Encode_DMA' makes pointer from integer without a cast [-Wint-conversion]
56 | #define CAMERA_FRAME_BUFFER ((uint32_t)0xD0600000)
| ^~~~~~~~~~~~~~~~~~~~~~
| |
| long unsigned int
C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/main.c:162:41: note: in expansion of macro 'CAMERA_FRAME_BUFFER'
162 | JPEG_Encode_DMA(&JPEG_Handle, CAMERA_FRAME_BUFFER, &JPEG_File);
| ^~~~~~~~~~~~~~~~~~~
In file included from C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/main.c:23:
../../../CM7/Inc/encode_dma.h:31:58: note: expected 'FIL *' but argument is of type 'long unsigned int'
31 | uint32_t JPEG_Encode_DMA(JPEG_HandleTypeDef *hjpeg, FIL *bmpfile, FIL *jpgfile);
| ~~~~~^~~~~~~
C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/main.c: At top level:
C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/main.c:79:13: warning: 'SD_Initialize' defined but not used [-Wunused-function]
79 | static void SD_Initialize(void)
| ^~~~~~~~~~~~~
C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/main.c:52:17: warning: 'LCD_X_Size' defined but not used [-Wunused-variable]
52 | static uint32_t LCD_X_Size = 0;
| ^~~~~~~~~~
arm-none-eabi-gcc -o "BSP_CM7.elf" @"objects.list" -l:libPDMFilter_CM7_GCC_wc32.a -mcpu=cortex-m7 -T"C:\_AMI\H747I-Disco\PGtestingH747\BSP\STM32CubeIDE\CM7\STM32H747XIHX_FLASH.ld" --specs=nosys.specs -Wl,-Map="BSP_CM7.map" -Wl,--gc-sections -static -L../../../Middlewares/ST/STM32_Audio/Addons/PDM/Lib --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -Wl,--end-group
C:/ST/STM32CubeIDE_1.15.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.200.202406191623/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: ./Example/User/CM7/encode_dma.o: in function `JPEG_Encode_DMA':
C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM7/Debug/../Example/User/CM7/encode_dma.c:113: undefined reference to `BMP_GetInfo'
C:/ST/STM32CubeIDE_1.15.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.200.202406191623/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM7/Debug/../Example/User/CM7/encode_dma.c:114: undefined reference to `JPEG_GetEncodeColorConvertFunc'
C:/ST/STM32CubeIDE_1.15.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.200.202406191623/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: ./Example/User/CM7/encode_dma.o: in function `JPEG_EncodeOutputHandler':
C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM7/Debug/../Example/User/CM7/encode_dma.c:149: undefined reference to `f_write'
C:/ST/STM32CubeIDE_1.15.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.200.202406191623/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: ./Example/User/CM7/encode_dma.o: in function `ReadBmpRgbLines':
C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM7/Debug/../Example/User/CM7/encode_dma.c:277: undefined reference to `f_lseek'
C:/ST/STM32CubeIDE_1.15.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.200.202406191623/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/_AMI/H747I-Disco/PGtestingH747/BSP/STM32CubeIDE/CM7/Debug/../Example/User/CM7/encode_dma.c:278: undefined reference to `f_read'
C:/ST/STM32CubeIDE_1.15.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.200.202406191623/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: ./Example/User/CM7/main.o: in function `main':
C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/main.c:140: undefined reference to `f_mount'
C:/ST/STM32CubeIDE_1.15.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.200.202406191623/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/main.c:161: undefined reference to `f_open'
C:/ST/STM32CubeIDE_1.15.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.200.202406191623/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/main.c:168: undefined reference to `f_close'
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:68: BSP_CM7.elf] Error 1
"make -j12 all" terminated with exit code 2. Build might be incomplete.
12:15:38 Build Failed. 9 errors, 5 warnings. (took 1s.946ms)
2024-08-07 5:50 AM
Yes, that is the full log. Here is the first error:
../Example/User/CM7/encode_dma.c: In function 'JPEG_Encode_DMA':
../Example/User/CM7/encode_dma.c:113:3: warning: implicit declaration of function 'BMP_GetInfo'; did you mean 'BSP_QSPI_GetInfo'? [-Wimplicit-function-declaration]
113 | BMP_GetInfo(pBmpFile, &Conf);So BMP_GetInfo is not declared yet. It should be declared before being used, typically by #including a header file. Find out which header file it's defined in and include it.
Similarly, f_write, f_lseek, and f_mount are also not defined anywhere.
You can use Search -> File... to find out where these are defined.
2024-08-07 6:40 AM
As you suggested I tried to do that, and included everything,
I still have this error:
In file included from C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/sdram.c:20:
../../../CM7/Inc/main.h:121: warning: "JPEG" redefined
121 | #define JPEG 1
|
C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/main.c: In function 'main':
C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/main.c:128:3: warning: statement with no effect [-Wunused-value]
128 | JPEG_InitColorTables;
| ^~~~~~~~~~~~~~~~~~~~
C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/main.c:131:25: warning: assignment to 'JPEG_TypeDef *' from 'int' makes pointer from integer without a cast [-Wint-conversion]
131 | JPEG_Handle.Instance = JPEG;
| ^
In file included from ../../../Drivers/BSP/STM32H747I-DISCO/stm32h747i_discovery.h:32,
from ../../../CM7/Inc/main.h:30:
../../../CM7/Inc/stm32h747i_discovery_conf.h:56:35: warning: passing argument 2 of 'JPEG_Encode_DMA' makes pointer from integer without a cast [-Wint-conversion]
56 | #define CAMERA_FRAME_BUFFER ((uint32_t)0xD0600000)
| ^~~~~~~~~~~~~~~~~~~~~~
| |
| long unsigned int
C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/main.c:161:41: note: in expansion of macro 'CAMERA_FRAME_BUFFER'
161 | JPEG_Encode_DMA(&JPEG_Handle, CAMERA_FRAME_BUFFER, &JPEG_File);
| ^~~~~~~~~~~~~~~~~~~
In file included from C:/_AMI/H747I-Disco/PGtestingH747/BSP/CM7/Src/main.c:23:
../../../CM7/Inc/encode_dma.h:31:58: note: expected 'FIL *' but argument is of type 'long unsigned int'
31 | uint32_t JPEG_Encode_DMA(JPEG_HandleTypeDef *hjpeg, FIL *bmpfile, FIL *jpgfile);
| ~~~~~^~~~~~~
../Example/User/CM7/encode_dma.c: In function 'BMP_GetInfo':
../Example/User/CM7/encode_dma.c:121:5: warning: implicit declaration of function 'LCD_SizesErrorDisplay' [-Wimplicit-function-declaration]
121 | LCD_SizesErrorDisplay();
| ^~~~~~~~~~~~~~~~~~~~~
../Example/User/CM7/encode_dma.c:303:13: error: invalid storage class for function 'ReadBmpRgbLines'
303 | static void ReadBmpRgbLines(FIL *file, JPEG_ConfTypeDef Conf, uint8_t * pDataBuffer, uint32_t *BufferSize)
| ^~~~~~~~~~~~~~~
../Example/User/CM7/encode_dma.c:319:1: error: expected declaration or statement at end of input
319 | }
| ^
../Example/User/CM7/encode_dma.c: At top level:
../Example/User/CM7/encode_dma.c:88:13: warning: 'ReadBmpRgbLines' used but never defined
88 | static void ReadBmpRgbLines(FIL *file, JPEG_ConfTypeDef Conf, uint8_t * pDataBuffer, uint32_t *BufferSize);
| ^~~~~~~~~~~~~~~(I hope I brought enough context for it)
I manually tried to fix the issue by including the relevant .h file inside this specific .c file. and even after I made the IDE recognize every type in there the compiler still gave me this error
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.