2019-09-02 9:34 PM
if someone can tell me how to write a byte to a FMC memory ?
Reading a 16bit word looks correct and I can read the status correctly
but using A0 as register select, this is writing one 16bit word,
it seems to write 4 times, A0 is jumping up and down,
It doesn't work on my external LCD chip.
2019-09-03 1:36 AM
Is the FMC area in question cached?
JW
2019-09-03 3:33 PM
Yes, the Data cache is turned off.
will check your link,
yes it is fixed now.
thanks for that
void MPU_Config(void)
{
MPU_Region_InitTypeDef MPU_InitStruct = {0};
/* Disables the MPU */
HAL_MPU_Disable();
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER7;
MPU_InitStruct.BaseAddress = 0x60000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_32B;
MPU_InitStruct.SubRegionDisable = 0x0;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/* Enables the MPU */
HAL_MPU_Enable(MPU_HFNMI_PRIVDEF);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.