2013-01-14 12:53 AM
Hi, I am currently porting robotics software from STM32F1 (Cortex M3) to STM32F4 (Cortex M4). I want to write a simple program to switch on an LED via digital out. The program is supposed to send a digital input interrupt from a pushbutton and output to LED when it is pressed. Somehow I cannot get my digital input configuration to work. I get strange result, which is, I can only initialize GPIO pin for input from GPIO-E Pin 0. After this, initialization does not work. Even if I only used Pin 0 in my code, it does not work. So I commented off initialization for the rest of the pins and use polling technique for Pin 0 (if-else button is pushed, turn off LED). It still does not work. Any idea where to look?
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;
GPIO_InitStructure.GPIO_OType = GPIO_OType_OD; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0; GPIO_Init(GPIOE, &GPIO_InitStructure); // Initialize pin 0 //CODE DOES NOT WORK BELOW THIS POINT GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1; GPIO_Init(GPIOE, &GPIO_InitStructure); // Initialize pin 1 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2; GPIO_Init(GPIOE, &GPIO_InitStructure); // Initialize pin 2 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3; GPIO_Init(GPIOE, &GPIO_InitStructure); // Initialize pin 3 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4; GPIO_Init(GPIOE, &GPIO_InitStructure); // Initialize pin 4 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5; GPIO_Init(GPIOE, &GPIO_InitStructure); // Initialize pin 5 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; GPIO_Init(GPIOE, &GPIO_InitStructure); // Initialize pin 6 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7; GPIO_Init(GPIOE, &GPIO_InitStructure); // Initialize pin 7 #gpio-digital-in2013-01-14 1:39 AM
It always helps to be more specific with ''does not work''.
JW2013-01-14 2:09 AM
+Works - When I place a function DIGITALOUT_On(LED2); or DIGITALOUT_Off(LED2); below that line, the function executes what it is supposed to to
+Does not work - function does not light up/turn off LED when function is placed below the line i used the LED out function as a breakpoint to locate precisely where the error is first I figured out that inside main.c, DIGITALIN_Config(); is causing problems. Then I look inside my digitalin.c file and i located that below GPIOE Pin 0 (see above code), for some reason the rest of the code causes problems. No idea why this is so. initially the light up routine used interrupt with function callback, but I wanted to narrow down the problem so I used polling. So, I bypass DIGITALIN_Config() entirely by using GPIO_ReadInputDataBit(GPIOE, GPIO_Pin_0); and if it returns 1, DIGITALOUT_On(LED2) should light up LED2. i.e. if the pin detects a high which means button is pressed, light up LED2. Even when using this method the LED does not turn on/off as it should. I am running out of explanations for why it is.2013-01-14 4:13 AM
What is DIGITALOUT_On() and the other functions you are mentioning?
Try posting a minimal program but complete enough to be compilable, exhibiting the problem. JW2013-01-14 6:31 AM
Double Post - Stupid Forum
2013-01-14 6:32 AM
Pin initialization looks Ok, need to look elsewhere for where your real problem lies.
It might be more simply accomplished with :GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 |GPIO_Pin_1 |
GPIO_Pin_2 |
GPIO_Pin_3 |
GPIO_Pin_4 |
GPIO_Pin_5 |
GPIO_Pin_6 |
GPIO_Pin_7
; GPIO_Init(GPIOE, &GPIO_InitStructure);02013-01-14 7:13 PM
This should be about it... Any help on where it went wrong? Where do I look?
--------------------- void DIGITALOUT_Config(void) { GPIO_InitTypeDef GPIO_InitStructure;RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOE, ENABLE);
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;
GPIO_Init(GPIOE, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9; GPIO_Init(GPIOE, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; GPIO_Init(GPIOE, &GPIO_InitStructure);GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11;
GPIO_Init(GPIOE, &GPIO_InitStructure); }void DIGITALOUT_On(char LEDx)
{ switch(LEDx) { case LED1: GPIO_SetBits(GPIOE, GPIO_Pin_8); break; case LED2: GPIO_SetBits(GPIOE, GPIO_Pin_9); break; case LED3: GPIO_SetBits(GPIOE, GPIO_Pin_10); break; case LED4: GPIO_SetBits(GPIOE, GPIO_Pin_11); break; } } void DIGITALOUT_Off(char LEDx) { switch(LEDx) { case LED1: GPIO_ResetBits(GPIOE, GPIO_Pin_8); break; case LED2: GPIO_ResetBits(GPIOE, GPIO_Pin_9); break; case LED3: GPIO_ResetBits(GPIOE, GPIO_Pin_10); break; case LED4: GPIO_ResetBits(GPIOE, GPIO_Pin_11); break; } }char DIGITALIN_Get(char DINx)
{ char ret=0; switch(DINx) { case PUSHBUTTON1: ret = GPIO_ReadInputDataBit(GPIOE, GPIO_Pin_0); break; case PUSHBUTTON2: ret = GPIO_ReadInputDataBit(GPIOE, GPIO_Pin_1); break; case PUSHBUTTON3: ret = GPIO_ReadInputDataBit(GPIOE, GPIO_Pin_2); break; case PUSHBUTTON4: ret = GPIO_ReadInputDataBit(GPIOE, GPIO_Pin_3); break; case DIPSWITCH1: ret = GPIO_ReadInputDataBit(GPIOE, GPIO_Pin_4); break; case DIPSWITCH2: ret = GPIO_ReadInputDataBit(GPIOE, GPIO_Pin_5); break; case DIPSWITCH3: ret = GPIO_ReadInputDataBit(GPIOE, GPIO_Pin_6); break; case DIPSWITCH4: ret = GPIO_ReadInputDataBit(GPIOE, GPIO_Pin_7); break; } return ret; }int main(void)
{ SYSTEM_Config(); DIGITALOUT_Config(); DIGITALOUT_On(LED1); DIGITALOUT_On(LED2); DIGITALOUT_On(LED3); DIGITALOUT_On(LED4);GPIO_InitTypeDef GPIO_InitStructure;
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOE, ENABLE); GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN; GPIO_InitStructure.GPIO_OType = GPIO_OType_OD; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0; GPIO_Init(GPIOE, &GPIO_InitStructure); // Initialize pin 0 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1; GPIO_Init(GPIOE, &GPIO_InitStructure); // Initialize pin 1 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2; GPIO_Init(GPIOE, &GPIO_InitStructure); // Initialize pin 2 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3; GPIO_Init(GPIOE, &GPIO_InitStructure); // Initialize pin 3 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4; GPIO_Init(GPIOE, &GPIO_InitStructure); // Initialize pin 4 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5; GPIO_Init(GPIOE, &GPIO_InitStructure); // Initialize pin 5 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; GPIO_Init(GPIOE, &GPIO_InitStructure); // Initialize pin 6 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7; GPIO_Init(GPIOE, &GPIO_InitStructure); // Initialize pin 7DIGITALIN_CallBack_PushButton1 = NULL;
DIGITALIN_CallBack_PushButton2 = NULL; DIGITALIN_CallBack_PushButton3 = NULL; DIGITALIN_CallBack_PushButton4 = NULL; while (1) { SYSTEM_Task(); if (DIGITALIN_Get(PUSHBUTTON1)!=0) { DIGITALOUT_Off(LED2); } else { DIGITALOUT_On(LED2); } } }What is DIGITALOUT_On() and the other functions you are mentioning?
Try posting a minimal program but complete enough to be compilable, exhibiting the problem. JW2013-01-14 10:39 PM
2013-01-14 11:27 PM
tried it.. no effect. am really perplexed.
2013-01-15 12:25 AM
What is
SYSTEM_Task()
? What happens if you drop it? And what about a simple blinkey, i.e. just toggle the LED with loop delay in between - does that work? JWWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.