2015-11-26 11:24 PM
I'm using the GNU ARM plugin for Eclipse with Open OCD as a debugger. This is on Windows 10 x64. The problem I'm facing is the following error when trying to debug or run the sample program:
Error in final launch sequence Failed to execute MI command: load C:\\Development\\stm32-test\\Debug\\stm32-test.elf Error message from debugger back end: Load failed Failed to execute MI command: load C:\\Development\\stm32-test\\Debug\\stm32-test.elf Error message from debugger back end: Load failed Load failed There are several kinds of STM32 project templates that the ARM plugin offers. Most notably, there's the ''STM32Fxxx C/C++ project'', and it works out of the box no problem. But it's bundled with the old version of STM32 library. I wanted to use the latest STM32F3Cube, so I used the other template - ''Hello World ARM Cortex-M C/C++ project'', as per the recommendation ofhttp://www.carminenoviello.com/en/2015/06/04/stm32-applications-eclipse-gcc-stcube/
. It's designed for use with the STM32F3Cube, and it's the one I can't load onto the board. Please tell me what further information is needed for dealing with this issue, or how I can collect more detailed logs etc. I'm in urgent need of a working project skeleton. Thanks in advance. P. S. I have compared the debug configuration settings between the working and non-working projects, and found no difference. Same .cfg file, along with everything else. Is my .elf being rejected because there's something wrong with it? #debugging #stm32f3discovery2015-11-27 1:55 AM
Found the problem: I didn't notice that I also need to edit the flash origin address in the mem.ld script. It's mentioned in the article I referred to, but I missed it. Doing that solved the issue.
2015-11-27 2:47 AM
Hi giraffe.violet,
Thank you for posting your findings and how you fixed the issue, it is good to hear that it was solved. -Syrine-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.