2016-02-25 1:36 AM
Hello everyone,
I have trying to reading axies from my accelerometer and I keep getting 0 from my X Y Z axies at movement.Have someone encounter this problem?My code:void writeTo(u8 addressToWrite,uint8_t value, u8 address){ I2C_start(I2C3, address, I2C_Direction_Transmitter); I2C_write(I2C3,addressToWrite); I2C_write(I2C3,value); I2C_stop(I2C3);} void setup(){ writeTo(DATA_FORMAT, 0x0B, WRITE_ADDRESS_1); writeTo(POWER_CTL, 0x08, WRITE_ADDRESS_1); writeTo(INT_ENABLE, 0x80, WRITE_ADDRESS_1);} void ReadOperation(uint8_t address){ I2C_start(I2C3, WRITE_ADDRESS_1 , I2C_Direction_Transmitter); I2C_write(I2C3,address); I2C_stop(I2C3);}void ReadFromAccel(){ ReadOperation(DATAX); I2C_start(I2C3,READ_ADDRESS_1 , I2C_Direction_Receiver); //Normal Reading and then offset Accel_Param.X_1 = I2C_read_nack(I2C3); Delay(0xFFFFa); ReadOperation(DATAY); I2C_start(I2C3,READ_ADDRESS_1 , I2C_Direction_Receiver); //Normal Reading and then offset Accel_Param.Y_1 = I2C_read_nack(I2C3); Delay(0xFFFFa); ReadOperation(DATAZ); I2C_start(I2C3,READ_ADDRESS_1 , I2C_Direction_Receiver); //Normal Reading and then offset Accel_Param.Z_1 = I2C_read_nack(I2C3); Delay(0xFFFFa);}//void ReadFromAccel() //Try to read all the axies together//{// ReadOperation(DATAX);// I2C_start(I2C3,READ_ADDRESS_1 , I2C_Direction_Receiver); //Normal Reading and then offset// Accel_Param.X_1 = I2C_read_ack(I2C3);// Accel_Param.Y_1 = I2C_read_ack(I2C3);// Accel_Param.Z_1 = I2C_read_nack(I2C3);// Delay(0xFFFFa);//}void ResetAccel(){ int i; inti_RCC(); init_I2C3(); GLB_DelayUs(1100); //need delay of 1.1 ms setup(); GLB_DelayUs(11000); //need delay of 11.1 ms for(i =0; i< 100; i++) //For noise { ReadFromAccel(); } for(i =0; i< 100; i++) { ReadFromAccel(); }} void I2C_start(I2C_TypeDef* I2Cx, uint8_t address, uint8_t direction){ // wait until I2C3 is not busy anymore while(I2C_GetFlagStatus(I2C3, I2C_FLAG_BUSY)); // Send I2C3 START condition I2C_GenerateSTART(I2C3, ENABLE); // wait for I2C3 EV5 --> Slave has acknowledged start condition while(!I2C_CheckEvent(I2C3, I2C_EVENT_MASTER_MODE_SELECT)); // Send slave Address for write I2C_Send7bitAddress(I2C3, address, direction); if(direction == I2C_Direction_Transmitter){ while(!I2C_CheckEvent(I2C3, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED)); } else if(direction == I2C_Direction_Receiver){ while(!I2C_CheckEvent(I2C3, I2C_EVENT_MASTER_RECEIVER_MODE_SELECTED)); }} void I2C_write(I2C_TypeDef* I2Cx, uint8_t data){ I2C_SendData(I2C3, data); // wait for I2C3 EV8_2 --> byte has been transmitted while(!I2C_CheckEvent(I2C3, I2C_EVENT_MASTER_BYTE_TRANSMITTED));} void I2C_stop(I2C_TypeDef* I2Cx){ // Send I2C3 STOP Condition I2C_GenerateSTOP(I2C3, ENABLE); while(!I2C_CheckEvent(I2C3, I2C_EVENT_MASTER_BYTE_TRANSMITTED)); }// read one byte and don't request another byte, stop transmissionuint8_t I2C_read_nack(I2C_TypeDef* I2Cx){ uint8_t data; // disable acknowledge of received data // nack also generates stop condition after last byte received I2C_AcknowledgeConfig(I2Cx, DISABLE); I2C_GenerateSTOP(I2C3, ENABLE); // wait until one byte has been received while( !I2C_CheckEvent(I2Cx, I2C_EVENT_MASTER_BYTE_RECEIVED) ); // read data from I2C data register and return data byte data = I2C_ReceiveData(I2Cx); return data;}2016-02-25 5:11 AM
Its work now.
I have called the registers of the ofset instead of the DATA.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.