STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Getting wrong axies from my accelormeter

Posted on February 25, 2016 at 10:36Hello everyone,I have trying to reading axies from my accelerometer and I keep getting 0 from my X Y Z axies at movement.Have someone encounter this problem?My code:void writeTo(u8 addressToWrite,uint8_t value, u8...

Writting to Flash memory on STM32F10xx

Posted on February 25, 2016 at 10:22Hello everyone! I'm trying to store a user data in flash memory by the nexf source code #define FLASH_START_ADDR  ((uint32_t)0x08000000) #define FLASH_END_ADDR      ((uint32_t)0x0803FFFF) #define FLASH_PAGE_SIZE  ...

tyr0 by Associate II
  • 1319 Views
  • 2 replies
  • 0 kudos

Stm32 dma question

Posted on February 25, 2016 at 08:39I use stm32f407 microcontroller and  I have a problem with spi send DMA mode.I use send data to vs1011 chip . when I use send data without DMA , Play sound wihout any problem. but when I enable DMA , vs1011 chip c...

STM32F091 Power and Speed

Posted on February 25, 2016 at 10:28Hello everybody and thanks for your help.I have been reading a document called: UM1724 STM32 Nucleo 64 boards User Manual and although very useful (more than other documents) it still left me a little confused so ...

d_aliaga by Associate II
  • 1186 Views
  • 1 replies
  • 0 kudos

AES implementation in STM32L0 series

Posted on February 25, 2016 at 11:27Hello,I need advice about AES 128 or AES 256 implementation in STM32L0 series. What is the best solution? Do I have to use the controller with AES hardware accelerator or there is a software solution that is fast ...

STM32F427 flash memory dual bank switching

Posted on February 25, 2016 at 09:14I am trying to live upgrade the firmware i.e. download firmware in bank 2 of flash memory while bank 1 is still executing the code and vice versa. I need to give starting address of flash memory where the new firm...

STM32F407 internal I/O circuit

Posted on February 25, 2016 at 09:22Hello everyone, i have a circuit where 8 I/O (5V tolarant)pins of my STM32F407(supply is 3.3V) are configured as inputs and are tied to 5V with a 10K pull-up resistor. The I/O as inputs work ok but when a configur...

td by Associate II
  • 1314 Views
  • 2 replies
  • 0 kudos

STM32 Nucleo. Problems with RESET

Posted on February 17, 2016 at 01:15Hello and thanks alwaysI am programming a STM32 Nucleo with mbed and I have a curious situation. If it sounds familiar to you, I would appreciate any pointer, advice or commentI have successfully programmed the nu...

d_aliaga by Associate II
  • 2495 Views
  • 3 replies
  • 0 kudos

STM32F103VB TWO USART Comm Simultaneously

Posted on February 24, 2016 at 15:21Hi,I am using stm32f103vb discovery board. Here i want to access UART1 and UART2 simultaneously. I have done coding in which i am able to transmit and receive data either through UART1 or UART2. But not able to en...

santhosh by Associate
  • 1408 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.