2016-02-24 7:02 AM
Hello together,
I have some problems with the IWDG of the STM32F103RBT6. I hope you can help me. The initialization: // Clear reset flags if( RCC_CSR & (1 << 29)) { RCC_CSR |= (1<<24); } /* Configure the watchdog */ IWDG_KR = 0x5555; /* Configuration access enabled */ IWDG_PR = 0x0002; /* Prescaler code 2: divider /16 */ IWDG_KR = 0x5555; IWDG_RLR = 0x04E2; /* 0x04E2 = 1250, f=40kHz, -> 1250 * 16 / 40000 = 500ms*/ IWDG_KR = 0xCCCC; The IWDG is cyclic triggered by: IWDG_KR = 0xAAAA; If the program runs into an infinite loop for testing the ''IWDGRSTF'' flag of the RCC_CSR register is set. But then the watchdog does not reset the controller, it still hungs in the infinite loop. The both bits of the status register ''IWDG_SR'' (RVU, PVU) are not set the whole time. Do you have any idea what I'm doing wrong? Thank you! Best regards from Germany FD #stm32-iwdg-watchdog-problem2016-02-24 7:44 AM
a) you're doing the test in a debugger, and there is some DBG MCU setting in effect.
b) you're driving the NRST pin high externally.2016-02-25 6:31 AM
Hi,
thank you, b) was the reason why it doesn't work! The NRST pin was connected directly to 3.3V. I think it should work with a series resistor between NRST and 3.3V. Best regards FDWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.