2024-03-18 8:30 PM
Hi I m using SPI to transmit and receive data from a sensor, the sensor return 3 bytes of data, SensorRXBuff[0], SensorRXBuff[1], and SensorRXBuff[2], i m gona use these 3 byte for indivual computation, i enclosed the function below, could anyone advise if this function is correct? is the uint_16 in front of function correct? how can i call the 2nd byte i.e SensorRXBuff[1]?
uint16_t Sensor(uint8_t *ch)
{
uint16_t SensorTxBuff[2] = {0x8, 0xAF};
HAL_GPIO_WritePin(..) // SPI CS low
if (HAL_SPI_TransmitReceive(&hspi1,(uint8_t *)&SensorTxBuff, (uint8_t *)&SensorRXBuff, 3, 100) != HAL_OK);
{
Error_Handler();
}
Hal_GPIO_WritePin;(...)// SPI CS hi..
return SensorRXBuff;
}please advise...
2024-03-19 12:06 AM
NO, it is NOT correct!
You define an uint16_t buffer for TX, but the SPI function sends all as a uint8_t buffer:
You will get the second byte as ZERO!
Your SensorTxBuff[2] has at the end as a uint8_t buffer used and sent by the SPI function this content:
0x8, 0, 0xAF, 0 #16bit words as little endian, because it is uint16_t!
But you send this buffer with 3 bytes (!), so that SPI will send: 0x8, 0, 0xAF (where does the 3 comes from?)
The second byte in SensorRxBuff is SensorRxBuff[1] (all starts from index 0).
I guess your code is not a "real code": why do you use &SensorTxBuff? It should be just SensorTxBuff (because it is an array and already the address of the buffer), or you had to use &SensorTxBuff[0] (the address location of the first entry).
Try to understand buffers, their addresses, how to access elements of the array (via [INDEX]) and in particular what "type casting" is, what happens, what the endian is...
(you are asking about "basic coding rules", not about how to use SPI... LOL)
2024-03-19 12:32 AM
Hi thx, the SPI transmit portion is working, i m able to receive 3 bytes from the sensor (ADC), the above code was modify to obtain the indiviual 3 received bytes, cos i need to compete the 2nd byte ie. SensorRXBuff[1].
could you advise what should the code be to churn out the 2nd receive byte from the SensorRXBuff ? thx.
void Sensor(uint8_t *ch)
{
uint16_t SensorTxBuff[2] = {0x8, 0xAF};
HAL_GPIO_WritePin(..) // SPI CS low
if (HAL_SPI_TransmitReceive(&hspi1, (uint8_t *)&SensorTXBuff, (uint8_t *)&SensorRXBuff, 3, 100) != HAL_OK)
{
Error_Handler();
}
HAL_GPIO_WritePin(..); // SPI CS high
}
2024-03-19 1:01 AM
Sure, sending 3 bytes via SPI in "full-duplex mode" gives you 3 bytes received.
As mentioned: the second byte received is SensorRxBuf[1].
uint8_t secondByteReceived;
secondByteReceived = SensorRxBuf[1];You can also do:
uint16_t secondWordReceived;
secondWordReceived = SensorRxBuf[1];But watch out here again: if you receive a byte via SPI, e.g. as 0x12 - the (16bit) word in secondWordReceived is 0x0012. When you dump the memory location (as bytes), you will see: 0x12, 0x00 (little endian).
Sorry, it does not look reasonable for me to define unit16_t with two values - which gives you 4 bytes and then to send just 3 bytes via SPI. OK, you get 3 bytes. And I am sure, you send 3 bytes, but the second one is a ZERO you send.
2024-03-19 1:23 AM
uint32_t Sensor(uint8_t *ch)
{
...
return SensorRXBuff;
}ok what should the function be? uint32_t and to return with SensorRXBuff ?
2024-03-19 1:31 AM
"I am lost":
SensorRxBuff is an address - not a value from the content of the buffer.
uint32_t Sensor(uint_t *ch)
{
//...
return (uint32_t)SensorRxBuff[1];
}would make much more sense, right?
Do you know how to handle types, casts, elements of an array (buffer)...?
2024-03-19 7:52 PM
I tried your suggestions but compiler report error @
uint32_t Sensor(uint_t *ch)
conflicting types for "Sensor"; have "uint32_(uint8_t*)" {aka 'long unsigned int(unsigned char*)'}
return (uint32_t)SensorRxBuff[1];
syntax error... pls advise thx...
2024-03-20 10:13 AM
I assume SensorRxBuff is not known in function Sensor. What is your entire function code?
Using *ch as the buffer - sure, it has to be something like this:
uint32_t Sensor(uint8_t *ch)
{
//...
return *(ch +1);
//or, depending what you do with pointer ch:
ch++;
return *ch;
//even tbis would return the 2nd element of the buffer ch:
return *(++ch);
//or this:
return ch[1];
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.