2010-10-21 12:20 AM
Frequncy counter on STM32
2011-05-17 5:12 AM
Yes I want measure frequency/duty of an external signal (from two external sources).
I heard that I can do so by using the PWM input mode for a timer 1 or 2.
But I can not write this in the software.
Can You help me in this case... Andrew2011-05-17 5:12 AM
Hi andrew,
Do you want to measure the frequency/duty of an external signal ? I remembre that there is an example provided by ST that shows how to measure signal frequency. Herzlich, MCU Lüfter2011-05-17 5:12 AM
Hi andrew,
There is an example provided by ST that shows how to measure signal frequency. Check it then tell me ... MCI Lüfter,2011-05-17 5:12 AM
I can not find the example. Can you show me the example?
Is it in Application Note?2011-05-17 5:12 AM
2011-05-17 5:12 AM
Hi arkar,
You can download the ST library from the link below: http://www.st.com/stonline/stappl/resourceSelector/app?page=resourceSelector&doctype=FIRMWARE&FamilyID=141 The name is ''ARM based 32-bit MCU STM32F1xx standard peripheral library'' The example is located in: STM32F10x_StdPeriph_Lib_V3.4.0/Project/STM32F10x_StdPeriph_Examples/TIM/PWM_Input Good luck,Herzlich,MCU Lüfter
2011-05-17 5:12 AM
Vielen Dank.
Frohe Weihnachten und guten Rutsch ins Jahr 2011 :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.