2018-02-09 12:42 AM
I would like to develop HMI hardware using STM32F746 with 480x272 Graphical LCd, But i have confusion on selection of Graphical LCD?Am i select Graphical LCD with graphic controller or without graphic controller? STM32F746 inbuilt LCD controller.
2018-02-13 12:37 PM
ER-TFT070-4 800 * 480, one contact 3.3V power supply digital part. RGB 8 * 8 * 8. 18 dollars.
The minimum headache when connecting to the st chip, without additional intermediate interfaces.A large resolution weakly improves image quality, but very well increases the price. On sale there are RGB displays without a built-in D / A converter and a high-voltage stabilizer - from $ 4. Such cheap displays can be used in the presence of experience in analog circuitry.
2018-02-13 12:39 PM
I used STM32F769 for control GLCD with RGB interface.
I tried control GLSD 800x480 with SSD1963 controller.
It is very very slow to fill screen1-2 sec for 800x480.
My project for SSD1963
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.