2018-12-21 7:54 PM
With the help of STM32 CUBEMX generated basic code for IAR-EW and I have design a small code to print float variables on UART for debug purpose in STM32F413RH. This is working fine in IAR-EW but same things when I used in Atollic TrueStudio it is not working. So, is there any specific setting or add some plugins may required in TureStudio?. Can you help me on this.
2018-12-21 8:37 PM
Search on Google and found that it is require to following setting in TrueStudio.
Under the project properties, find the C/C++ build->Settings->Tool Settings->C Linker->Miscellaneous->Other options option in the air: -u_printf_float.
After doing this it is working fine.
Apart from this setting anything may required?.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.