2017-03-13 9:01 PM
Fellow Programmers, STMicro Staff, and CubeMX Coding Team:
After a whole day of debugging, I found an error in CubeMX code generation that results in FIFO errors from DMA when streaming to DAC. How soon can CubeMX be corrected? It is a nuisance to edit the generated C file to fix the bug every time after CubeMX is used to generate new code again.
Here are the details:
(1) DMA -> DAC normal trigger from any timer, with Interrupts enabled for DAC errors.
(2) CubeMX generates file 'STM32F7xx_HAL_DMA.C' file, with line 486 setting the FIFO Error Interrupt Enable (which is a mistake) even though FIFO Mode is supposed to be disabled.
(3) CubeMX Generated code looks like this ...
/* Enable Common interrupts*/
hdma->Instance->CR |= DMA_IT_TC | DMA_IT_TE | DMA_IT_DME; hdma->Instance->FCR |= DMA_IT_FE; // Mistake - Always enable FIFO Error contradicting FIFOMode setting(4) Generated code should be like this ...
/* Enable Common interrupts*/
hdma->Instance->CR |= DMA_IT_TC | DMA_IT_TE | DMA_IT_DME; if (hdma->Init.FIFOMode == DMA_FIFOMODE_ENABLE) // If FIFOMode enabled { hdma->Instance->FCR |= DMA_IT_FE; // Only enable FIFO Errors if FIFOMode enabled }(5) With this CubeMX code-generation error, I have to ask why is the hardware even generating an error since the FIFOMode has been set to disabled? Where does this FIFOMode change the hardware operation?
(6) Does this mean that FIFO errors will always occur when FIFOMode is required to be enabled?
I think there is a hardware problem here as well. Please confirm what is going on.
Thanks,
Garry Anderson.
2017-03-21 6:12 AM
Hello,
I will share your issue internally with CubeMx team for check and we come back to you as soon as possible.
About hardware problem, you can check if you have the same conditions in the errata sheet related to your device.
Imen
2017-03-21 7:52 AM
>>How soon can CubeMX be corrected?
It is generally unwise to set critical path requirements on third-parties, especially unpaid ones, they tend to have their own time lines and agendas. The tools have been in the process of being 'corrected' for several years now.
I would suggest sandboxing your stable design, and merging in changes if you use CubeMX in an iterative fashion
2017-10-11 1:43 AM
I have This Problem.
2017-10-12 4:22 AM
Use a little sed script that is called before the build or manually just after you regenerate the code that rewrites the relevant lines.
Install a sed tool from somewhere out there in net land...
Put the following in a file called dma.sed
's/hdma->Instance->FCR |= DMA_IT_FE;/if (hdma->Init.FIFOMode == DMA_FIFOMODE_ENABLE) { hdma->Instance->FCR |= DMA_IT_FE; }/g'
Create a batch file containing::-
rename
STM32F7xx_HAL_DMA.C
STM32F7xx_HAL_DMA.C
XXpath to sed -f dma.sedSTM32F7xx_HAL_DMA.C
XX >STM32F7xx_HAL_DMA.C
delSTM32F7xx_HAL_DMA.C
XXRun it after a regenerate.
I have a number of these 'Fixes' in my codebase...
Andy
2017-10-30 3:30 AM
Hello,
Is there any reply from CubeMX Team yet?
I have the same problem, when i use the ADC and an SPI with DMA toghether. The SPI TX DMA has a high priority and ADC a low priority. If I use only SPI (ADC is not configured), everything is working correctly. But when I also configure ADC with DMA, the SPI DMA is getting the FIFO Error eventhough FIFO is disabled at ADC and SPI.
By disabling FIFO Interrupt in function 'HAL_DMA_Start_IT' it works fine.
Dani
2017-11-10 12:54 AM
Thanks! This solved my problem as well. I kept getting the FIFO error even though fifomode was disabled. I fixed it by adding the following line after HAL_ADC_Start_DMA
// Start ADC1 with DMA
if(HAL_ADC_Start_DMA(&adc_handle, (uint32_t*)adc_values, 16) != HAL_OK) {
printf('error hal_adc_start_dma');
}
// Manually disable fifo interrupt.
dma_handle.Instance->FCR = 0U;
2017-11-22 12:59 AM
Hi Imen,
Any progress on this? We're also seeing a similar issue when using DMA for UART TX (with no FIFO enabled). When disabling DMA_IT_FE everything works as expected. Is that the right way to do it?
What I can't understand is how a UART TX DMA could ever trigger a FIFO error. Even if the DMA is busy for a long time, it should just send the data when possible, there should never be any errors involved here? On RX I can understand, but not TX.
It seems that it's especially sensitive to this issue if calling HAL_UART_Transmit_DMA() directly inside the HAL_UART_TxCpltCallback() callback. I'm not sure why this would make any difference though.
/Peter
2018-05-04 3:40 AM
Hi
Anderson.Garry
,As reminder, the following is part of RM0431 Reference manual, 'STM32F72xxx and STM32F73xxx advanced Arm®-based 32-bit MCUs'
... In direct mode, the FIFO error flag can also be set under the following conditions: • In the peripheral-to-memory mode, the FIFO can be saturated (overrun) if the memory bus is not granted for several peripheral requests. • In the memory-to-peripheral mode, an underrun condition may occur if the memory bus has not been granted before a peripheral request occurs. ... Note: When a FIFO overrun or underrun condition occurs, the data is not lost because the peripheral request is not acknowledged by the stream until the overrun or underrun condition is cleared. If this acknowledge takes too much time, the peripheral itself may detect an overrun or underrun condition of its internal buffer and data might be lost.Disabling FIFO error is going to prevent from being informed of underrun.
Before doing this, please may you check that the stream priority of the DMA is enough high.As information, development team fed back that it is planned in next deliveries (end of the year):
- FIFO error will be de-activate as default configuration in interrupt mode - a new service will be created to set DMA_IT_FE in hdma->Instance->FCR, if one wants to be informed of such errors.Hopping it clarifies and may you confirm this thread is completed.
Regards.
Cyril
2018-05-04 11:00 PM
Hi Cryil:
Have you considered that the DAC is being driven by DMA Peripheral, therefore “underrun� or “overrun� is impossible, unless the hardware design is faulty.
So please have your development team try to figure out how the FIFO error can even occur with DMA as the controller. Either the DMA is faulty or the DAC is faulty.
Thanks,
Garry.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.