2025-06-13 7:01 AM
Hi ST Community,
I’m working on a CAN FD project using the STM32H753VIT6 and facing a limitation with data phase bitrate while using Bit Rate Switching (BRS).
Controller: STM32H753VIT6
FDCAN clock source: PLL1Q
PLL1Q output: 40 MHz
Frame format: CAN FD with BRS (FDCAN_FRAME_FD_BRS)
Nominal (arbitration) bitrate: 1 Mbps
Target data bitrate: 2 Mbps or higher
Despite the configuration, I'm not able to achieve more than ~1.92 Mbps on the data phase. Even when I reduce the number of time quanta or adjust prescalers, the speed does not increase beyond this limit.
Is there any known limitation when using PLL1Q = 40 MHz for FDCAN clock?
Is the STM32H753 internal FDCAN limited to certain bitrates per kernel clock frequency?
Could internal synchronization or sampling constraints prevent achieving the expected 2.5 Mbps from a 40 MHz FDCAN clock?
Attachments:
main.c file
Oscilloscope screenshot showing BRS waveform and time base
STM32CubeMX clock configuration screenshot
Any insights or suggestions would be greatly appreciated!
Thanks in advance,
Pavan
Solved! Go to Solution.
2025-06-19 2:08 AM
You didn't answer that question: did you try with the Loopback mode?
2025-06-19 3:16 AM
Yes, I used external loopback mode to test the configuration, and I was able to achieve stable communication at both 5 Mbps and 8 Mbps data phase bitrates. I verified the bitrates using a DSO by measuring the bit duration.
2025-06-19 3:43 AM
Did you activate the delay compensation?:
/**
* Configure and enable Tx Delay Compensation, required for BRS mode.
* TdcOffset default recommended value: DataTimeSeg1 * DataPrescaler
* TdcFilter default recommended value: 0
*/
if (HAL_FDCAN_ConfigTxDelayCompensation(&hfdcan1, (hfdcan1.Init.DataPrescaler * hfdcan1.Init.DataTimeSeg1), 0U) != HAL_OK)
{
Error_Handler();
}
if (HAL_FDCAN_EnableTxDelayCompensation(&hfdcan1) != HAL_OK)
{
Error_Handler();
}
Please refer to this Github link linked to this article: STM32 FDCAN running at 8 Mb/s on NUCLEO boards
2025-06-19 4:31 AM
At first, I had not enabled Tx Delay Compensation. After your suggestion, I enabled it as recommended for CAN FD with Bit Rate Switching (BRS) mode. As a result, I was able to achieve communication at 8 Mbps.
Thank you for your valuable guidance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.