2025-06-13 7:01 AM
Hi ST Community,
I’m working on a CAN FD project using the STM32H753VIT6 and facing a limitation with data phase bitrate while using Bit Rate Switching (BRS).
Controller: STM32H753VIT6
FDCAN clock source: PLL1Q
PLL1Q output: 40 MHz
Frame format: CAN FD with BRS (FDCAN_FRAME_FD_BRS)
Nominal (arbitration) bitrate: 1 Mbps
Target data bitrate: 2 Mbps or higher
Despite the configuration, I'm not able to achieve more than ~1.92 Mbps on the data phase. Even when I reduce the number of time quanta or adjust prescalers, the speed does not increase beyond this limit.
Is there any known limitation when using PLL1Q = 40 MHz for FDCAN clock?
Is the STM32H753 internal FDCAN limited to certain bitrates per kernel clock frequency?
Could internal synchronization or sampling constraints prevent achieving the expected 2.5 Mbps from a 40 MHz FDCAN clock?
Attachments:
main.c file
Oscilloscope screenshot showing BRS waveform and time base
STM32CubeMX clock configuration screenshot
Any insights or suggestions would be greatly appreciated!
Thanks in advance,
Pavan
Solved! Go to Solution.
2025-06-19 3:43 AM
Did you activate the delay compensation?:
/**
* Configure and enable Tx Delay Compensation, required for BRS mode.
* TdcOffset default recommended value: DataTimeSeg1 * DataPrescaler
* TdcFilter default recommended value: 0
*/
if (HAL_FDCAN_ConfigTxDelayCompensation(&hfdcan1, (hfdcan1.Init.DataPrescaler * hfdcan1.Init.DataTimeSeg1), 0U) != HAL_OK)
{
Error_Handler();
}
if (HAL_FDCAN_EnableTxDelayCompensation(&hfdcan1) != HAL_OK)
{
Error_Handler();
}
Please refer to this Github link linked to this article: STM32 FDCAN running at 8 Mb/s on NUCLEO boards
2025-06-13 10:50 AM
Hello,
I don't think there is a limitation 40Mhz vs bitrate > 2Mb/s
Refer to this article: STM32 FDCAN running at 8 Mb/s on NUCLEO boards on which we showed that we can reach 8Mb/s in data phase.
Check also your transceiver bandwidth.
Meanwhile refer to this article: FAQ: Fixing STM32 FDCAN communication disruptions - APB bus, kernel, and time quanta clocks and check if you are in the same situation
2025-06-13 11:05 AM
Thank you for your response.
My transceiver bandwidth is 5 MHz for FDCAN and 1 MHz for classic CAN.
I followed the same clock configuration as mentioned, but I'm still unable to achieve a speed beyond 2 Mbps. Could you please suggest the best approach to troubleshoot this issue? If there’s a possibility of any mistake in my configuration or code, I would really appreciate your guidance.
Thanks again.
2025-06-13 11:22 AM
Were you able to achieve the target bitrate in Loopback mode?
2025-06-13 11:54 AM
No, I did not measure the actual bitrate during the external loopback test. I used that mode only to verify the basic communication functionality. Without confirming the exact timing parameters, I proceeded to normal mode, where I am currently testing the communication between two transceivers on the same STM32H753 device. Specifically, I am transmitting from FDCAN1 and receiving on FDCAN2, and then vice versa.
My primary goal is to evaluate the maximum achievable data rate in a real physical setup using CAN FD with Bit Rate Switching (BRS). I have configured PLL1Q at 50 MHz (the max supported for FDCAN on this device), and I am using 64-byte payloads with proper timing configurations.
Could you please guide me on:
The best practices for achieving and validating the maximumFDCAN speed on STM32H7?
How to accurately measure and verify the bitrate during transmission.
2025-06-13 11:55 AM
Please test the loopback mode before to proceed ..
2025-06-13 12:28 PM
Sure, I will test the loopback mode before proceeding. Just to confirm, which loopback mode would be more suitable in my case — internal loopback or external loopback?
2025-06-13 12:31 PM - edited 2025-06-13 12:32 PM
External loopback with the same clock and CAN configs and probe CAN_Tx
2025-06-15 1:59 AM - edited 2025-06-15 2:02 AM
I think You have set the Data baudrate wrong. If You have set the FDCAN Clock to 50MHz then Your setup:
hfdcan1.Init.NominalPrescaler = 1;
hfdcan1.Init.NominalSyncJumpWidth = 4;
hfdcan1.Init.NominalTimeSeg1 = 86;
hfdcan1.Init.NominalTimeSeg2 = 13;
hfdcan1.Init.DataPrescaler = 1;
hfdcan1.Init.DataSyncJumpWidth = 2;
hfdcan1.Init.DataTimeSeg1 = 10;
hfdcan1.Init.DataTimeSeg2 = 2;will result in:
Nominal Bitrate: 50e6/(1+86+13) = 500e3 (500kBit)
Data Bitrate: 50e6/(1+10+2) = 3.8462e6(!)
if You want 500KBit/2Mbit You have to cange the Data segment's (for example 20 and 4)
2025-06-19 2:05 AM
i already set this with 50 MHz. but I don't get more than 1.92 mbps"
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.