2017-05-30 1:56 AM
Hello,
By using the STM32Cube_FW_F4_V1.16.0, there is the FatFs which is provided by default as third party software. I see that the version of that FatFs is very old: R0.11. There are 6 new fixes that occurred since then and it improved things a lot. Also there is the exFat which is now supported.
Changelog:
http://elm-chan.org/fsw/ff/updates.txt
Website:
http://elm-chan.org/fsw/ff/00index_e.html
Would it be possible to update the latest release into CubeF4 middleware? I think that this should also be done with all other middleware, so people have directly the best products available freely.
Thank you.
2017-05-30 2:30 AM
Hi
Burgin.Daniel
,Your request is shared internally for further investigation.
I'll keep you update about the answer.
Thanks
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.