2017-05-29 11:50 PM
Actually I am working with a STM32L433CBY controller. When using the internal temperature sensor I got some inconsistencies and strange readings. Maybe someone can clarify the issues.
1. Reference temperature TS_CAL2
The
explains on page 40 both calibration points. TS_CAL2 is defined to be 130�C.The
introduces on page 423 (center) the formula for using the calibration points. Here TS_CAL2 is defined to be 110�C.Any Idea which value is the correct one?
2. Oversampling
I get different values when enabling 16x oversampling for the ADC. At room temperature (~25�C, VCC=3.3V) I get an ADC reading (after a division by 16) of 0x2FE. When I deactivate oversampling I get 0x343 for the same temperature on the same hardware. Is there any limitation regarding oversampling of the internal temperature sensor? Did I miss something in the errata sheet? (PS: Tried it also on different controllers, same result.)
3. Unrealistic readings of the temperature sensor
When I fill in the values from (2) into the formula, I get quite strange results. First I converted the readings into millivolts to compare them to page 155 of the datasheet. The datasheet states that I should get about 0.76V at 30�C.
0x02FE ==> 620mV (much too low, even for 25�C)
0x0343 ==> 670mV (better but still to low!)
When I use these values for the formula (RM0394, pp423) with the calibration values
TS_CAL1 = 1031
TS_CAL2 = 1371I first have to normalize the readings to 3.0V (since the calibration was done at that voltage).
TS_DATA = 0x343(=835) * 3,3V / 3,0V ==> 0x396 (=918)
T = (110�C-30�C) / (1371 - 1031) * (TS_DATA - 1031) + 30�C
= 80�C / 340 * (TS_DATA - 1031) + 30�C = 0,235�C * (TS_DATA - 1031) + 30�C = 0,235�C * -113 + 30�C = 3,44�C (*brrr, coooold*)When replacing TS_CAL2=110�C with TS_CAL2=130�C I get
T = 0,294�C * (TS_DATA - 1031) + 30�CT = 0,294�C * -113 + 30�CT = -3,2�C (*coooolder*)Any ideas what's going wrong?
Carsten
#temperature-sensor #adc-stm32l4 #stm32l42017-05-30 12:14 AM
Can you tell what hardware (board) you are working on ?
I don't have any L4xx board, but I vividly remember some peculiarities of other discovery boards.
These boards could be powered by either USB (via the ST-Link part), external 5V, external 3.3V, and sometimes even via target USB. And all these supply sources were decoupled via Shottky diodes, which made for a 'floating' supply voltage, below the specified 3.3V.
If one used Vcc as reference for the ADC on those boards, similar problems arose. Perhaps applies to your case.
2017-05-30 2:25 AM
The board is a custom PCB. Voltage is derived from a 5V Supply (bench PSU) using a linear regulator on the board. The 3V3 is quite stable.
Analog parts are decoupled from digital parts using a ferrite. Blocking capacitors are present near the uC according to the hardware guide.
When I did the tests, the only enabled peripherals were RCC (for PLL), ADC and DMA.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.