2021-05-25 1:50 PM
Hello,
I would like to know the behavior of the BOOT0 pin on a factory fresh STM32G474 device. I'm wondering if I can use PB6 as a general input without causing side effects if the flash option register is at factory defaults. The reference manual shows: "Reset value: 0xFXXX XXXX", but what are the *** *** values as shipped from the factory?
Thank you for any insight you can provide - much appreciated!
Regards,
Dave
Solved! Go to Solution.
2021-05-26 7:07 AM
Hi Bassett.David,
This register is loaded from option bytes. The "ST production value" for option bytes is written in reference manual RM0440 (chapter FLASH option bytes). For FLASH_OPTR (and STM32G474 device) is the ST production value: 0xFFEF F8AA .
Regards
Igor
2021-05-26 7:07 AM
Hi Bassett.David,
This register is loaded from option bytes. The "ST production value" for option bytes is written in reference manual RM0440 (chapter FLASH option bytes). For FLASH_OPTR (and STM32G474 device) is the ST production value: 0xFFEF F8AA .
Regards
Igor
2021-05-26 7:27 AM
Hello Igor,
Thank you very much! I apologize for missing it. (In RM0440 Rev. 6, I was looking at page 138, but the information I needed was on page 110).
Regards,
Dave
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.