2012-03-26 7:03 AM
Hi, I not having much success with using the UART (USART1) on my F4Discovery board (STM32F407). I am pretty new to STM32 and Keil (the IDE I am using). Here's my code:
&sharpinclude ''stm32f4_discovery.h''
&sharpinclude ''stm32f4xx_usart.h'' &sharpinclude ''stm32f4xx.h'' void usartSetup(void); void USART_PutChar(uint8_t ch);int main (void) {
usartSetup();USART_PutChar(0); //I realise this won't send a 0
USART_PutChar(8); //I realise this won't send an 8 USART_PutChar(255); //I realise this won't send a 255while (1) {
//loop forever } }void usartSetup (void) {
USART_InitTypeDef USART_InitStructure; //USART_StructInit(&USART_InitStructure); USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART1, &USART_InitStructure); USART_Cmd(USART1, ENABLE); }void USART_PutChar(uint8_t ch) {
USART_SendData(USART1, (uint16_t) 0x49); while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); USART_SendData(USART1, (uint16_t) 0x49); }I'd be very grateful if someone could help. It never sends the 0x49 out of the UART1 TX (have checked pin PA9 and PB6) and then gets endlessly stuck on the while(USART_GetFlagStatus...). I am observing using the Keil debugger and see it get stuck in the while. I also have a scope probe on the TX pin and never see anything.
I am including the stm32f4xx_usart.c driver into the project.
Thanks!
#rs232-uart-usart-f4discover-407 #uart #stm32f4discovery2012-05-01 12:14 PM
Now you're mixing it up with DMA.
When polling, you need to wait on RXNE for EACH character. Your st[] array has no size to it, if you want 20 characters you need to allocate space for them.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.