2010-02-05 12:47 AM
EXTI detection on STM32F103VET6
2011-05-17 4:39 AM
Seems you get interrupts from port A, huh?
Use GPIO_EXTILineConfig(port, pin) to configure the mapping right.2011-05-17 4:39 AM
Hi Edison,
thanks for your replay. I already used GPIO_EXTILineConfig(port, pin) to set up the right port pin. But this was not working. After a closer look on this function i found that the parameter are not port and pin, i.e. GPIOB and GPIO_Pin_7. Instead of this they have to be GPIO_PortSourceGPIOB and GPIO_PinSource7 in this case. And with this it works like expected. I was only a bit confused because the function was working (or even not working) with the wrong parameters without any error message. I would have expect a compiler error. Best regards TomWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.