2023-05-16 3:43 AM
Hi
I follow the MOOC tutorial for create the external QSPI loader, my Flash memory is MT25QL128ABB.
The flash is writed but the memory test Fail, with debug inspect there is 1 byte shift from start 0x90000000 (currect 00 01 02 ecc) I read (01 02 03).
I don't know were is the problem , some parameters of flash ?
Solved! Go to Solution.
2023-05-16 4:51 AM
Thak I reduced DUMMY_CLOCK_CYCLES_READ_QUAD 8 and Work , Thank
2023-05-16 3:52 AM
Other problem thar the flash is not complete written , the MT25Ql128 is 32mB x 4 therefore from 0x90000000 + 0x1000000 but the pattern is wrote 0x9070000
extern QSPI_HandleTypeDef hqspi;
/* USER CODE BEGIN Private defines */
uint8_t CSP_QUADSPI_Init(void);
uint8_t CSP_QSPI_EraseSector(uint32_t EraseStartAddress, uint32_t EraseEndAddress);
uint8_t CSP_QSPI_WriteMemory(uint8_t* buffer, uint32_t address, uint32_t buffer_size);
uint8_t CSP_QSPI_EnableMemoryMappedMode(void);
uint8_t CSP_QSPI_Erase_Chip (void);
/* USER CODE END Private defines */
void MX_QUADSPI_Init(void);
/* USER CODE BEGIN Prototypes */
/*MX25L512 memory parameters*/
#define MEMORY_FLASH_SIZE 0x1000000 /* 128 MBits => 16MBytes */
#define MEMORY_BLOCK_SIZE 0x10000 /* 1024 sectors of 64KBytes */
#define MEMORY_SECTOR_SIZE 0x1000 /* 16384 subsectors of 4kBytes */
#define MEMORY_PAGE_SIZE 0x100 /* 262144 pages of 256 bytes */
/*MX25L512 commands */
#define WRITE_ENABLE_CMD 0x06
#define READ_STATUS_REG_CMD 0x05
//#define READ_FLAG_STATUS_REG_CMD 0x70
#define WRITE_STATUS_REG_CMD 0x01
#define SECTOR_ERASE_CMD 0x20
#define CHIP_ERASE_CMD 0xC7
#define QUAD_IN_FAST_PROG_CMD 0x38
#define READ_CONFIGURATION_REG_CMD 0x15
#define QUAD_READ_IO_CMD 0xEC
#define QUAD_OUT_FAST_READ_CMD 0x6B
#define QPI_ENABLE_CMD 0x35
#define DUMMY_CLOCK_CYCLES_READ_QUAD 10
#define RESET_ENABLE_CMD 0x66
#define RESET_EXECUTE_CMD 0x99
#define DISABLE_QIP_MODE 0xf5
/* USER CODE END Prototypes */
#ifdef __cplusplus
}
#endif
2023-05-16 4:01 AM
So perhaps wrong commands, not in the right mode, or a disagreement on address width or dummy cycles.
2023-05-16 4:51 AM
Thak I reduced DUMMY_CLOCK_CYCLES_READ_QUAD 8 and Work , Thank
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.