2020-11-09 1:55 PM
Hi,
Is there any one success with ESP-PSRAM64H in memory mapped mode?
We are able to read ID (0x9F) in spi mode. But when we read/write, it return 0xFF. We don't see EnableWrite command, does this chip has EnableWrite command?
We also wanted to use this memory as RAM so we can read and write from a pointer.
But how we send Read and Write command Id at the same time when set register at memory mapped mode?
Many thanks
2020-12-08 2:31 AM
Hi,
The QuadSPI memory Controller of the STM32H743 is a NOR memory Controller and so it doesn't support Memory Mapped Write function
Other version of STM32H7 (for example H7A3/B3/B0 or H72x/73x) does support full functionality of of QSPI or OPI RAM
Alex
By the way, the ESP-PSRAM64H is only supporting ESP32, equivalent Quad RAM PN to use is APS6404L-3SQR-SN (16Mb or other package also available)
2021-01-08 4:25 AM
If you only want to read and write, you can use a STM32H743:
Using an ESP-PSRAM64H with a STM32H743:
https://github.com/koendv/micropython-psram
If you want to do memory-mapping, you need a STM32H7A3:
https://github.com/koendv/micropython-spiram
but I am still working on that.
2021-01-08 5:43 AM
Hi,
If you don't need the Memory Mapped Write mode, you can use the NOR Memory controller of STM32H743 to drive the Quad PSRAM (this is not officially supported/tested by STM, formally support NOR not RAM, but we have multiple customer using it for Quad PSRAM). Please note ESP-PSRAM64H is only valid to be used in combination of ESP32, so you should use APS6404L-3SQR-SN.
Yes for the full Quad (APSxx04x-xSQR-xx) or Octal (APSxx08x-xOBx-xx) PSRAM support, you can use the latest version of STM32 series such as STM32L5, STM32L4P5/Q5, STM32H7A3/B3, STM32H72x/3x. If you are looking for reference, the STM32L4P5G-DK has both QSPI and OPI PSRAM foot print on board (https://www.st.com/content/st_com/en/products/evaluation-tools/product-evaluation-tools/mcu-mpu-eval-tools/stm32-mcu-mpu-eval-tools/stm32-discovery-kits/stm32l4p5g-dk.html)
Alex
2021-01-24 2:50 AM
I am afraid reading the errata is fruitful on this one.
After experimenting with a single 64Mbit qspi psram on stm32h7a3:
Terminal ready
spiram eid 0d 5d 52 a2 64 31 91 31
spiram memtest16 fail, address 0x903e2070 written 0x5a5a read 0x0000
MicroPython v1.13-260-g0b108aaa0-dirty on 2021-01-24; DEVEBOX STM32H7XX with STM32H7A3If I connect a logic analyser to the qspi bus, I see the data going from processor to spi ram is occasionally corrupt: when I do a write, sometimes some bytes still have the value from before the write. This seems to be a cache issue. I'm not aware of a workaround. Correct me if I'm wrong.
Source code used.
2022-03-30 5:59 AM
Dear koendv, We have also chosed stm32h7a3 and APS6404L-3SQR. We have exactly the same problem using ospi and memory mapping in write mode. I wonder if you managed to solved the problem? If so, can you please share it with us?
Artin
2022-03-30 6:07 AM
Hi Artin,
STM32H7A3 won't support QSPI SDR RAM mapped memory write.
But OSPI is running well, so alternative if manageable could be 64Mb OPI BGA24 3V APS6408L-3OBM-BA (or 128Mb QSPI DDR 1.8V WLCSP)
Regards
Alex
2022-03-30 6:42 AM
Dear Alex,
Do you mean that APS6404L-3SQR and STM32H7A3 doesn't work in OSPI/quad mode and memory mapping?
/Artin
2022-03-30 6:47 AM
Hi Artin,
Correct, it support all functions, except Memory Mapped Write in Quad SDR
Quad DDR or OPI works full spec
Can you deal with OPI memory device APS6408L-3OBM-BA ?
Regards
Alex
2022-03-30 6:53 AM
Dear Alex,
Thanks a lot for the reply! I will try to test it with APS6408L-3OBM-BA if we have enough pins. Is there any sample code for it for our STM32H7A3VIT?
/Artin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.