2014-03-16 8:52 PM
Hi,
I trying to use ST-LINK/V2 in STM32F4 discovery board to program an external application in SWD mode.I connected Pin GND, Pin 3.3V, Pin SWCLK, Pin SWDIO from external board to ST-LINK/V2 and remove connection from ST-LINK/V2 to CM4 chip in STM32F4 discovery board. I use Keil ARM and in CORTEX-M DRIVER SETUP window, tool can recognize ARM CORE SIGHT SW-DP. But when I load, tool flag : ''no taget connected''...Please, help me. Are there any note at external board, I put BOOT 0 and BOOT 1 on external boad to 0V.Thanks.2014-03-17 8:53 AM
Hi nguyen,
Please ensure that you have connected ST-Link correctly . if your application requires ''connect under reset'', you have to connect also the NRST pin. Please visit the technical documentation available on the web site at the following link :http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00039084.pdf
You can refer to the section :
4.2.2 Using ST-LINK/V2 to program/debug an external STM32 application
Best Regards, Nouha
Hi,
I trying to use ST-LINK/V2 in STM32F4 discovery board to program an external application in SWD mode. I connected Pin GND, Pin 3.3V, Pin SWCLK, Pin SWDIO from external board to ST-LINK/V2 and remove connection from ST-LINK/V2 to CM4 chip in STM32F4 discovery board. I use Keil ARM and in CORTEX-M DRIVER SETUP window, tool can recognize ARM CORE SIGHT SW-DP. But when I load, tool flag : ''no taget connected''... Please, help me. Are there any note at external board, I put BOOT 0 and BOOT 1 on external boad to 0V. Thanks.2014-03-22 2:52 AM
Hi Nouha,
Thanks for your help,I connect Reset pin together and it's ok. But now, I met problem when conect STLINK V2 with another board, I config hardware as last time and ''Stm32 ST LINK Unility'' tool show the error ''cannot connect to device, MCU is kept under reset''. Please, show me the solution.Thanks and regards,Nhan Nguyen2014-04-01 6:35 AM
Hi Nhan Nguyen,
Please Check you Reset pin : it should be high. let me know. Best Regards, Nouha2014-04-01 8:21 AM
Please, show me the solution.
Generally you'll have issues if the part is not powered/functional, or user code is doing something abherant preventing JTAG/SWD access. You can remove user code from the equation by pulling BOOT0 High at reset. Your other method to confirm signs-of-life is to use the USART to connect to the System Loader. This may require you read some documentation, and become familiar with the tools.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.