STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

creating header in a project

Posted on April 01, 2014 at 19:22Hello everybody, I have a problem in a project, I want to compilate a code, it has worked correctly in another project ( but the another project is not mine), the code is a simple delay. Here is the body of my code.d...

STM32F2xx Save User Data (ie virtual eeprom)

Posted on April 01, 2014 at 02:45I have been attempting to store a few bytes in some non-volatile memory on the STM32fxx. From what I understand, there are two places to save data that does not require vbat battery backup... I may be out to lunch, b...

dj by Associate II
  • 2933 Views
  • 6 replies
  • 0 kudos

adding regular function to the _it.c file

Posted on April 01, 2014 at 16:44hi,i added a function ( not an ISR )  to the stm32f4xx_it.c file.when i call it from main() i couldn't program the .elf file to the target ( using the segger )  getting ''no source available for 0x0''.does someone kn...

worlag by Associate II
  • 1447 Views
  • 2 replies
  • 0 kudos

STM32F4 USART receive problem

Posted on October 25, 2012 at 07:33 Hi, I'm having problems receiving USART data on the F4. I can see the data is being sent from my LCD on my Saleae logic analyser, but the STM32 won't call the USART RXNE interrupt. I can send data no probl...

FILE stream for ITM redirect

Posted on April 01, 2014 at 14:00 Hi everyone! My question is in short: how can I set up a FILE stream for using it like the stdout and stderr to with the ITM trace facility. My question explained in more detail: My syst...

rigomate2 by Associate III
  • 847 Views
  • 0 replies
  • 0 kudos

STM32W108: SWO trace not working

Posted on March 26, 2014 at 20:06 Hello, I cannot start SWO trace (nothing received in debug window) with STM32 W108CB. I have standard configuration of ITM, listed below. And i configured the 33 pin for SWO with line ''REG_GPIOC->CRL ...

gsegment by Associate
  • 1302 Views
  • 2 replies
  • 0 kudos

STM32F405 cannot connect using SWD

Posted on March 28, 2014 at 13:57I'm having the same problem as the one [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM32F4%20-%20No%20target%20connected&Folde...

mluessi by Associate II
  • 1374 Views
  • 1 replies
  • 0 kudos

STM32L-Discovery To STM32L-Discovery using SPI

Posted on September 20, 2013 at 21:41I am looking for some code to do a demo of the Touch Sensor and SPI. When TouchSesnsor on Board 1 is pressed. It's value is displayed on Board 2 lcd.  Any Ideas, or places I should look?Thanks  Chuck

STM32F0 TIMER + DAC + DMA!

Posted on March 19, 2014 at 06:29The original post was too long to process during our migration. Please click on the attachment to read the original post.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.