2021-02-08 4:55 PM
Howdy
this line:
hadc->Instance->CR |= ADC_CR_ADSTART;
at the end of:
HAL_ADC_Start_DMA(ADC_HandleTypeDef* hadc, uint32_t* pData, uint32_t Length);
is causing a crash / reset. I've used HAL for this set up quite a few times with no problems, but this time it wont survive enabling the regular conversion. Any ideas what's happening here? I am trying to configure more channels than I ever have before, 15. 14 pins and the vrefint internally. Using an STM32L071RBT6
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.