STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Write Backupcode from QSPi to SDRAM when flashing from IDE

My application is executed from flash and external SDRAM.I have a bootloader(seperat project) that saves the volatile SDRAM content on a QSPI.Normaly my application is applyed by a .hex file that is located on the SD-Card. So my bootloader can clearl...

Minti by Associate II
  • 713 Views
  • 0 replies
  • 0 kudos

STM32H753 ADC auto calibration not working properly?

I am using STM32H753 MCU. I am using ADC1 and ADC2 and calibrated the ADC offset using auto calibration function. But this function is not working properly. I am getting a difference of 50 counts on subsequent starts of my device. I checked this by g...

Akash_k by Associate III
  • 1269 Views
  • 1 replies
  • 0 kudos

Errors in STM32F446RE datasheet

Refer to https://www.st.com/resource/en/datasheet/stm32f446re.pdfIn section 3.23 on PDF page 32, it says:"The devices embed four universal synchronous/asynchronous receiver transmitters (USART1, USART2, USART3 and USART6) and four universal asynchron...

JArmi.1 by Associate II
  • 1159 Views
  • 1 replies
  • 0 kudos

Delay function using timers - LED blinks too fast

void delay_setup(void) { rcc_periph_clock_enable(RCC_TIM6); timer_set_prescaler(TIM6, rcc_apb1_frequency / 1000000 - 1); timer_set_period(TIM6, 0xffff); timer_one_shot_mode(TIM6); }   void delay_us(uint32_t us) { TIM_ARR(TIM6) = us; TIM_EGR(TIM...

BSerb by Associate II
  • 1442 Views
  • 1 replies
  • 0 kudos

Resolved! How to reset SPI interface after HAL_SPI_TransmistReceive_IT?

Hello,I'm working with a STM32F446 and I configured the SPI as slave.In my process I receive x bytes of data in interruption. But during the process, this size of data changes to y. But the function HAL_SPI_TransmitReceive_IT(x) has already been call...

Saredo by Associate III
  • 2175 Views
  • 1 replies
  • 0 kudos

using STM32L0538, is it possible to make SysTick_Handler count in microseconds not in milliseconds and if it is, where to start?

I'm writing some code with PWM and I'm using very high number of periods in short time causing my LED's to dim very choppy. I think it's not working properly because timer is to fast and counting in milliseconds and I need it to count in microseconds...

DSimp.1 by Associate III
  • 1618 Views
  • 4 replies
  • 0 kudos

Resolved! SPI slave 1 bit shift after power on

Hi, I'm working with a STM32F446ZET6. In this case, I configured my SPI as slave, and I use the HAL_SPI_TransmitReceive function.The problem is that when the slave shoud respond with the value 0x11, I receive 0x22 on the master side.I have checked th...

Saredo by Associate III
  • 2171 Views
  • 5 replies
  • 0 kudos

Resolved! P-NUCLEO-IHM002 doesn't run

I have a brand new P-NUCLEO-IHM002 out of box. I configured it according to the instruction. however, when power up, D11 on IHM07M1 is not light at all. when i push the blue button, no response. LD3 on Nucleo-F302R8 is on, LD1 is flashing. Can you he...

SLi.11 by Associate II
  • 1572 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.