2019-10-29 2:25 AM
If I connect a constant rising signal at the ADC input, I observe significant fluctuations at certain ADC values. These fluctuations always appear at the same ADC values. The affected values have the following format XX500, e.g. 18500, 19500, 20500 etc.
I was also able to reproduce this behavior with the NUCLEO-H743ZI and the example projects (ADC_DMA_Transfer and ADC_RegularConversion_Polling) from the current cube firmware V1.5.0. The graphic in the appendix shows a recorded ADC values, which shows the problem.
Can someone help me to solve the problem?
Solved! Go to Solution.
2019-11-07 7:58 AM
2019-11-08 5:07 PM
Thanks for sharing! Looks better, but not entirely ok...
2019-11-21 11:37 PM
ADC clock how many M do you configure?
2019-11-21 11:38 PM
2019-11-21 11:39 PM
I also encountered this situation, the higher the configuration, the greater the signal impact
2019-11-21 11:40 PM
2019-11-25 1:19 AM
I have tried different ADC clock configurations. The dropouts will not disappear in this way.
2019-11-25 5:50 PM
Can you think that the ADC stability of H7 is not as good as that of F4?
2019-11-25 5:51 PM
F4's ADC is still very stable
2019-11-25 11:52 PM
I switched from F4 to H7 because F4 ADC had a lot of noise. With the same RC element and 12 bit value, I measured 3x higher noise with F4 than with H7.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.