2019-04-28 4:49 PM
I generated FOC code by 3 shunt from MCSDK5.3.3.
the base project comes from STM32CubeExpansion_SPN7_V1.1.0.
The MCU is STM32F302R7Tx.
Please review below code and respond the error.
static void MX_NVIC_Init(void)
{
/* TIM1_BRK_TIM15_IRQn interrupt configuration */
HAL_NVIC_SetPriority(TIM1_BRK_TIM15_IRQn, 4, 1);
HAL_NVIC_EnableIRQ(TIM1_BRK_TIM15_IRQn);
/* USART2_IRQn interrupt configuration */
HAL_NVIC_SetPriority(USART2_IRQn, 3, 1);
HAL_NVIC_EnableIRQ(USART2_IRQn);
/* ADC1_IRQn interrupt configuration */
HAL_NVIC_SetPriority(ADC1_IRQn, 2, 0);
HAL_NVIC_EnableIRQ(ADC1_IRQn);
/* EXTI15_10_IRQn interrupt configuration */
HAL_NVIC_SetPriority(EXTI15_10_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI15_10_IRQn);
}
2019-04-28 10:44 PM
If you breakpoint and look at the calling stack, what do you see?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.