STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! [Solved] STM32H743 SAI DMA Receiving only '0's

Hey,I configured the stm32h743 to transfer data with sai2 and read the same data with sai1. Sai2 is in IT mode and works fine (checked it with a logic analyzer).The SAI2 is totally working in IT mode, but when I put it in DMA mode i only receive 0's....

Resolved! STM32H743I-EVAL FDCAN can not receive

Posted on August 17, 2017 at 13:48Hello,    I tried the example 'FDCAN_Com_polling' on STM32H743I-EVAL, it worked like it should be.Then I separated the example code into TX part and RX part, made one of my STM32H743I-EVAL board as TX and another as...

RTC Date Lost after reset

HII use STM32F107RTC6 and configure for time and dateafter reset time is ok but date lost and reset to 2000/1/1please help me

HAkba by Associate
  • 1215 Views
  • 1 replies
  • 0 kudos

STM32F746 SDMMC VOLTAGE SWITCH

Hello,I am using STM32F746 discovery board with 16GB kingston UHS-1 card. I want to know whether SDMMC host supports 1.8V signalling level or not nothing is mentioned in RM about that. sorry if i missed out. which register of the host i should config...

n.serina by Associate III
  • 714 Views
  • 0 replies
  • 0 kudos

STM32H753I-EVAL board avaibility

I am looking for a STM32H753 evaluation board, this kind of board seems to be unvailable either on the ST site or the distributor site . Do you have some informations about this kind of evaluation board ? Where / when can I buy a STM32H753 evaluation...

YROSS by Associate II
  • 1453 Views
  • 2 replies
  • 0 kudos

doesn't reach infinite loop and stop in interrupt setting

I generated FOC code by 3 shunt from MCSDK5.3.3.the base project comes from STM32CubeExpansion_SPN7_V1.1.0. The MCU is STM32F302R7Tx.Please review below code and respond the error.static void MX_NVIC_Init(void){ /* TIM1_BRK_TIM15_IRQn interrupt confi...

MYu by Associate II
  • 1205 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.