2020-04-28 12:07 PM
It says specifically in datasheet that it does, but when I create new STM32CubeIDE project and select STM32F730V8, FMC only offers PSRAM/NOR Flash/LCD interface. I tried for testing purposes selecting some other MCU that also supposedly supports SDRAM, I did get a choice of selecting it. Am I doing something wrong?
Solved! Go to Solution.
2020-04-28 1:43 PM
I found one that is similar to one that you mentioned, STM32F730Z8T6. It's in stock on mouser.com. What's best way to program it? I was thinking about buying a dev board, but there isn't any with that particular MCU. Could I use a similar board and then use it for debugging external MCU?
2020-04-28 2:19 PM
What about voltages? SDRAM uses 1.8V, but MCUs are all at 3.3V. Do I need voltage level converter, or MCU does that automatically?
2020-04-28 2:50 PM
How do they do it on the Disco/EVAL boards?
JW
2020-04-28 3:37 PM
I have no idea. I'm planning yet to buy one.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.