2019-08-13 11:38 PM
Hi, does input frequency have effect on the smooth digital calibration period since in the documentation(screenshot attached) it says the calibration is performed during a cycle of 2 to the power of 20 which amounts to frequency of 32.768 x 32 . Does this change when the input frequency is 40.000 since both frequencies are configured with prescalers to 1 Hz. If it does, would I need to perform different calculations for number of clock pulses I want to mask/add?
Thank you for your response.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.