2023-10-08 11:28 PM
I have enabled two interrupts. First one is EXTI for GPIOA0 Pin and another is UART3 for RXCALLBACK.
I want to disable EXTI interrupt when UART interrupt is triggered and enable again EXTI interrupt once the task is completed.
I used __disable_irq(5) to disable the EXTI interrupt but I am seeing below error on building the project.
./Drivers/CMSIS/Include/cmsis_gcc.h:129:27: note: declared here
129 | __STATIC_FORCEINLINE void __enable_irq(void)
| ^~~~~~~~~~~~
Kindly suggest. I am still learning the interrupt handling. Not sure where I am wrong.
2023-10-09 1:30 AM
Hello @Nico3,
the __disable irq() function disables all interrupt, HAL_NVIC_DisableIRQ(IRQn) is probably what you're looking for!
Try that out, and keep us updated!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-10-09 1:42 AM
why disable exti ?
just put higher priority for uart , than exti. so exti will never disturb uart . :)
2023-10-12 11:03 AM
2023-10-12 11:06 AM
yes, I would like to implement but m confuse about priority implementation. I see vector table mentioned in datasheet has priority for each interrupt. But STM32 cubeide shows default 0 priority and can be selected in between only 0,1, 2.
Please clarify.
2023-10-12 11:23 AM - edited 2023-10-12 11:23 AM
Depends on how the NVIC is configured to group them, the M3/M4 implement 4-bits for priority/preemption levels and how those are split, 2-bits for each gives 4-levels.
Even at the same priority level the NVIC shouldn't call another interrupt whilst servicing the current one, it should simply tail-chain it next.
Not 100% sure on the CM0 STM32F0, perhaps look at ST's Programming Manual for the CM0(+) parts, or perhaps Joseph Yiu's treatment of the NVIC via one of his Essential Cortex-M books related to the CM0
2023-10-12 11:26 AM
2023-10-12 1:01 PM
Honestly there is no point in using the HAL bloat like the HAL_NVIC_DisableIRQ()/HAL_NVIC_EnableIRQ() functions. Just use the normal ARM CMSIS provided NVIC_DisableIRQ()/NVIC_EnableIRQ() functions.
2023-10-16 5:06 PM
thanks a lot ...Joesph guide gave me some clarity on NVIC..
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.