2023-10-16 2:43 PM
I've generated a CubeMX project for a mass storage class device and can't seem to get the OTG_FS embedded pullup on DP to engage. I've enabled VBUS sensing, and can confirm that the code initially does a soft disconnect (OTG_DCTL->SDIS = 1) then a connect (OTG_DCTL->SDIS = 0), then I get a VBUS sensing break-point when I plug into a PC (confirmed that OTG_DTCL-> still is 0), but I never see the pullup engage so no enumeration.
Is it true that after the initial soft disconnect and when SDIS = 0, then the pullup should engage when VBUS appears without code intervention?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.