2016-10-22 7:36 AM
Hello,
I am having an issue with DFU downloading to a STM32L476 Discovery board.- Compiled a simple LED switching application in IAR converted to DFU by the file manager (tried both bin and hex)- Tested via ST-LINK - works fine- Connected BOOT0 to 3V - the board presented itself as DFU- Downloaded DFU- removed BOOT0 connection, pressed reset - application does not startTried both DFUSe 3.0.5 and DFU tester in the package - same result - downloads but does not start. Also tried to set flash address to 0x080000000 during ''to bin'' conversion - no effect.What could be a problem? Any help would be appreciated.2016-10-29 2:16 AM
Hi ferentes,
It will be better to follow one only thread for the same subject. So, putting responses in this [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/DFU%20DFUSE%20problem%20with%20STM32L4%20%28STM32L476VG%29&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=19]thread.Regards2019-03-25 2:44 AM
Hi,
It looks like i am facing similar issue as reported in this post. For some reason i am not able to OPEN the link shared by @slimen . Could you please share working link. Your help is much appreciated.
Digging further, it looks to me like the last incomplete page (<2kBytes) of application image is not copied to STM32L476 FLASH at all when programmed using DFU mode.
Regards,
Suhel
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.