STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SDIO Hardware Flow Control

Posted on December 17, 2013 at 05:03Greetings all, I've been playing around with SDIO on an STM32F4 -Discovery card with the Embest Baseboard on it. My goal is to get it to work in polling mode, flow control mode, interrupt mode, and dma mode. This ...

orders-st by Associate II
  • 3345 Views
  • 2 replies
  • 0 kudos

STM32L4xx Internal RTC Timestamp

Hey, I try to get timestamp from tamper event when mcu supplied with VBAT, but value oftimestamp still 0, can anyone help me ?

dobs by Associate II
  • 1419 Views
  • 2 replies
  • 0 kudos

DFU and DFUSE for STM32L476 Discovery Problem

Posted on October 22, 2016 at 16:36Hello,I am having an issue with DFU downloading to a STM32L476 Discovery board.- Compiled a simple LED switching application in IAR converted to DFU by the file manager (tried both bin and hex)- Tested via ST-LINK ...

imalamoud by Associate II
  • 1287 Views
  • 2 replies
  • 0 kudos

STM32H743 errata

Posted on May 24, 2018 at 12:03I have designed a board using the STM32H743II. During integration testing of the software I have found the following issues related to the microcontroller (SCB->CPUID 0x411fc271) :1)SPI1 and ADC1 is not working when us...

Problem with SPI transmission on G071

Hi,I am having problems sending a part of an array with SPI. It is no problem to send 4 Bytes from the beginning of the array, but if I want to send 4 Bytes from another starting position (for example: start from tmp[1]) it does not work. In this cas...

BerndE by Associate II
  • 2223 Views
  • 5 replies
  • 0 kudos

STM32L4 Backup Domain Register

Hey, I want asking something, I have a value on backup register, but when the tamper is active when power off, the value on my backup register was reset. On datashet get to protect the backup domain no erase or mask flag bit must enable. I set the no...

dobs by Associate II
  • 602 Views
  • 0 replies
  • 0 kudos

STM32 + QT GUI Desktop

Hi,i use STM32CubeMX and Keil 5 for my embedded project and now I want to create a Desktop GUI using QT to command STM32,I want first to just create 4 buttons which correspond to 4 leds of the STM32F4 Disco Board,Please can anyone help me:Environm...

mmed by Associate III
  • 862 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.