2024-06-24 2:17 AM - last edited on 2024-06-24 7:26 AM by mƎALLEm
while (1) {
if (DmaRecHalfBuffCplt == 1) {
/* Store values on Play buff */
for (int i = 0; i < 1024; i++) {
PlayBuff[2 * i] = (int16_t) SaturaLH((RecBuff[i] >> 8), -32768,
32767);
PlayBuff[(2 * i) + 1] = PlayBuff[2 * i];
}
HAL_UART_Transmit_DMA(&huart1, (uint8_t*) PlayBuff, 4096);
DmaRecHalfBuffCplt = 0;
}
if (DmaRecBuffCplt == 1) {
/* Store values on Play buff */
for (int i = 1024; i < 2048; i++) {
PlayBuff[2 * i] = (int16_t) SaturaLH((RecBuff[i] >> 8), -32768,
32767);
PlayBuff[(2 * i) + 1] = PlayBuff[2 * i];
}
DmaRecBuffCplt = 0;
}
/* USER CODE END WHILE */
}
I try to use the AudioTrack Android SDK api to play the PlayBuff data,but i saw The PlayBuff array consists mainly of repeated values FF 7F 80 00. What could be the reason for this?
2024-06-24 7:25 AM
Hello and welcome to the community.
Please read these recommendations on this link on how to post threads on this community, especially the posting of a code source.
Thank you for your understanding.
2024-06-24 8:04 PM
void MX_DFSDM2_Init(void)
{
/* USER CODE BEGIN DFSDM2_Init 0 */
/* USER CODE END DFSDM2_Init 0 */
/* USER CODE BEGIN DFSDM2_Init 1 */
/* USER CODE END DFSDM2_Init 1 */
hdfsdm2_filter0.Instance = DFSDM2_Filter0;
hdfsdm2_filter0.Init.RegularParam.Trigger = DFSDM_FILTER_SW_TRIGGER;
hdfsdm2_filter0.Init.RegularParam.FastMode = ENABLE;
hdfsdm2_filter0.Init.RegularParam.DmaMode = ENABLE;
hdfsdm2_filter0.Init.FilterParam.SincOrder = DFSDM_FILTER_SINC4_ORDER;
hdfsdm2_filter0.Init.FilterParam.Oversampling = 128;
hdfsdm2_filter0.Init.FilterParam.IntOversampling = 1;
if (HAL_DFSDM_FilterInit(&hdfsdm2_filter0) != HAL_OK)
{
Error_Handler();
}
hdfsdm2_channel1.Instance = DFSDM2_Channel1;
hdfsdm2_channel1.Init.OutputClock.Activation = ENABLE;
hdfsdm2_channel1.Init.OutputClock.Selection = DFSDM_CHANNEL_OUTPUT_CLOCK_AUDIO;
hdfsdm2_channel1.Init.OutputClock.Divider = 10;
hdfsdm2_channel1.Init.Input.Multiplexer = DFSDM_CHANNEL_EXTERNAL_INPUTS;
hdfsdm2_channel1.Init.Input.DataPacking = DFSDM_CHANNEL_STANDARD_MODE;
hdfsdm2_channel1.Init.Input.Pins = DFSDM_CHANNEL_SAME_CHANNEL_PINS;
hdfsdm2_channel1.Init.SerialInterface.Type = DFSDM_CHANNEL_SPI_RISING;
hdfsdm2_channel1.Init.SerialInterface.SpiClock = DFSDM_CHANNEL_SPI_CLOCK_INTERNAL;
hdfsdm2_channel1.Init.Awd.FilterOrder = DFSDM_CHANNEL_FASTSINC_ORDER;
hdfsdm2_channel1.Init.Awd.Oversampling = 1;
hdfsdm2_channel1.Init.Offset = 0;
hdfsdm2_channel1.Init.RightBitShift = 0x05;
if (HAL_DFSDM_ChannelInit(&hdfsdm2_channel1) != HAL_OK)
{
Error_Handler();
}
if (HAL_DFSDM_FilterConfigRegChannel(&hdfsdm2_filter0, DFSDM_CHANNEL_1, DFSDM_CONTINUOUS_CONV_ON) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN DFSDM2_Init 2 */
/* USER CODE END DFSDM2_Init 2 */
}
void HAL_DFSDM_FilterRegConvHalfCpltCallback(DFSDM_Filter_HandleTypeDef *hdfsdm_filter) {
DmaRecHalfBuffCplt = 1;
}
void HAL_DFSDM_FilterRegConvCpltCallback(DFSDM_Filter_HandleTypeDef *hdfsdm_filter) {
DmaRecBuffCplt = 1;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.