2021-02-24 3:42 AM
What are the possibilities t reduce the current cosumption at the beginning. Can you give me some information about basic mechanisms to throttle the required power especially in the boot process. Is there a documentation available regarding to this topic?
Thank you very much for your reply.
Best regards,
Johannes
2021-02-24 4:24 AM
What is the problem during your programm setup? High current or energy (current * time for setup) ? In the first case, switch to a lower frequency early in the setup. This will run longer, but with less current.
2021-02-24 4:31 AM
Identify where the peak consumption is occuring, ie have waypoints where you signal via GPIOs and plot that against the current consumption, that way you'll have a profile from which areas to focus on.
Initial clock sources
Starting different clock sources
Waiting for sources and PLLs to lock
Initializing, clearing and copying statics
2021-02-24 5:49 AM
> Especially at the beginning( Boot process) the current consumption is very high.
This is a relative statement.
How high is the current/power consumption, and what do you expect to see ?
Have you checked the datasheet ?
It specifies average currents for many operation modes, clock frequencies and environment temperatures.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.