2011-11-07 8:23 AM
Hello everyone,
I have had a couple porblems resolved by sharing with the community here. I am now moving into the toughest part of my project. I am incorporating a Micron VGA CMOS Digital Image Sensor that I have previously had working on an 8051 through an Altera FPGA chip. The image sensor only put out intersperesed 8 bit serial LVDS so I have it going through a de-serializer and all the signals look perfectly fine as expected. I have 1 byte of data the Pixel clock and H and V Syncs all wired into the STM3220g eval board, which has the F207IG on board. Now that the quick introduction is out of the way. Let me get started out with what I am seeing. I have DMA setup to transfer a picture into SRAM and this is happening, except for the fact that all my image data is exactly the same. The DMA is transferring 0x04040404 into memory as that is all that is put in the data register. I know this is not all the data that the camera is putting out as it I have it setup in test mode putting out a grayscale image. I know that it is seeing something from the camera though as it is not getting anythign in the data register when i disconnect the camera. I do notice some discrepencies between the memory map file and the reference manual from what I am actually seeing in the DCMI_SR. In Crossworks Studio I am seeing: DRDY CECS SECS CEIS SEIS Where in the reference manual it is showing: FNE VSYNCE HSYNC Has anyone else noticed these differences or know what the CECS,SECS, CEIS, SEIS may stand for? The DRDY, CECS, and SECS flags are the onse being set. When DRDY is set so is CECS, and SECS is reset. When SECS is set, DRDY and CECS are reset. Regarding my issue, I know I really didn't address with a question as I am a bit confused still with working with this DCMI. I will at keep everyone posted on my progress. Please if you have any experience using DCMI and are willing to share I am willing to read! Thanks, Brad2012-06-26 12:23 PM
Surely that should be
void DCMI_IRQHandler(void) unless you've changed it in the vector table source2012-06-27 11:38 AM
I tried as you suggest and finally interrupt occured but some wierd thing happend:)
I enabled frame caprute interrupt to check it.I simply write toggle some pin as an interrupt function.The wierd thing is toggling periode is only 300ns.I expected some thing like 30ms(for 30fps)I tried with different HS VS PCK polarities but i am not sure if it is the problem or not.Thanks for your help..2012-06-27 11:53 AM
Hello,
Do you have access to an oscilloscope? If possible look at VSYNC and HSYNC on there to confrm everythign is running as it should. As far as the polarities I had to flip them in the DCMI initialization. Though the fram is valid when VSYNC is high, I had to configure it as DCMI_InitStructure.DCMI_VSPolarity = DCMI_VSPolarity_Low;2012-06-28 1:20 AM
hi h.brad :)
i mentioned before that i used a logic analyzer to check signals.Both of them seems ok to me.i have a vsync pulse at every 40ms and 176 pulse between every vsync (i am using B&W QCIF).But data is streaming when VSYNC is low and HSYNC is high About polarities i configured sensor as default.so do you suggest that DCMI_InitStructure.DCMI_VSPolarity = DCMI_VSPolarity_High; DCMI_InitStructure.DCMI_HSPolarity = DCMI_VSPolarity_Low; well what about pclk polarity?i read data sheet but could not find pclk polarity and data streaming relaition. By the way still confused about interrupt periode :)2012-07-01 10:30 AM
http://spostimage.org/m80g77fwn/clk.jpg
I was collecting very meaningful data until i messed up my code:) According to me DMA and DCMI is fine.but as2012-07-03 5:11 PM
Check your camera's manual register set. From what I checked form 7740's there is a register in where you set the clock, vsync and hsync polarities, maybe there's the same with your camera.
But from your image all data is on polarity high ;)2012-08-11 4:54 AM
hi everyone
Im working on stm3240g eval board. I have some issues regarding JPEG. I get low res images in other formats on the LCD as well as on the SD card. But when I edit the code for Jpeg format I dunno what exactly I get.The data i get I ma unable to display it on the screen. i transferred it to the sd card. but then its in hex format(no FAT). in case of BMP images, there are direct converters from hex to bmp. I dunno what I am supposed to do in case of JPEG images. Any ideas??2013-07-17 2:41 PM
Hallo!
I'm working with the same devices. Did you managed a working code?If so, could you help me with dcmi-dma configuration?Thanks,JenoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.