STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

AN4013 & RM0313 contradict about Timer Features?

Posted on July 08, 2013 at 00:37Hello Forum, i am trying to get an overview of the various timer periphals present in the STM32 Mikrocontroller Family. It now seems that the two documents http://www.st.com/st-web-ui/static/active/cn/resource/technic...

profclonk by Associate II
  • 3584 Views
  • 7 replies
  • 0 kudos

STM32F427 - USART - most significant bits problem

Posted on July 17, 2013 at 08:59Hello,I'm trying to make a communication protocol via the UART. I have a M4 and an A8 which communicates via RS485 transmitters.For the trials, the UART is set to 9600 bps, 8 bits per character with one stop bit and a...

clement by Associate II
  • 1544 Views
  • 2 replies
  • 0 kudos

STM32F4 flash erase for IAP

Posted on July 04, 2013 at 14:53Hi everybody, I'm trying to make the IAP exampe code from ST running on the Olimex board E-407 (STM32F4) but when i want to erase the flash, a hardfault occurs. More precisely, it happens right after setting the STRT ...

lesaint by Associate
  • 2328 Views
  • 4 replies
  • 0 kudos

Problem with CAN config and Clock STM32F407VG

Posted on July 17, 2013 at 11:35 Hi, I have a problem with my CAN configuration, I try to interface the STM32 with a NI USB/CAN. The problem is the baudrate configuration I think, see my code below : GPIO_InitTypeDef GPIO_...

aurelien by Associate
  • 1228 Views
  • 2 replies
  • 0 kudos

Some problems with DCMI stm32f407vgt6 mcu

Posted on July 10, 2013 at 11:46I have some problems with DCMI (stm32f407vgt6 mcu).I saw on forums the examples of reading data from camera and sending it through DMA to LCD.What I want is to get the data from DCMI, save 1 frame to internal SRAM mem...

hitsumen by Associate II
  • 1373 Views
  • 2 replies
  • 0 kudos

TIMx as a watchdog timer?

Posted on February 02, 2012 at 18:07I need a ''watchdog timer'' that automatically sets a port pin when it times out and not reset the processor. I don't think the IWDG or WWDG do this since they just reset the processor on time-out. Therefore, I th...

gds23 by Associate II
  • 2882 Views
  • 6 replies
  • 0 kudos

SDADC1 does not work when start the DMA on STM32F373

Posted on July 18, 2013 at 04:17Hi,everyone I have a question about SDADC and DMA.when I enable the DMA with'' DMA_Cmd(DMA2_Channel3, ENABLE)'' in program and the SDADC1 stop convert immediately. here is my code:void SDADC1_Config()  {    SDADC_Init...

I2C1 issue when using PB6 and PB7

Posted on July 17, 2013 at 21:12 When using the Audio_Playback_and_record example I was able to communicate with the codec[UDA1380] I2C interface[PB6, PB9] but when using PB6 and PB7[on my own board], I get a NAK even though the data appears to ...

DCMI Issues, looking for insight.

Posted on November 07, 2011 at 17:23Hello everyone, I have had a couple porblems resolved by sharing with the community here. I am now moving into the toughest part of my project. I am incorporating a Micron VGA CMOS Digital Image Sensor that I hav...

stbbrad3 by Associate II
  • 15715 Views
  • 47 replies
  • 0 kudos

function for set reset

Posted on July 17, 2013 at 11:03HI , i have this function which sets x bit( passed as a parameter) of a byte . after some code the variable should be restored to it's initial value .char a ; global variable void function(char x){int b = a;a |= (1<<x...

raducara by Associate II
  • 1332 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.